Pulse Building

Generate

Generates a waveform for the pattern specified by Pattern to Generate property.

This command verifies the active pattern, creates the pattern signal data (including the waveform, sequence, and marker data), applies corrections, generates and downloads the signal to the signal generator's volatile waveform memory and sets up signal generator settings associated with the baseband signal and turns on the Arb. The signal generator then automatically plays the signal.

Example - When a pattern named "Pattern1" is generated, Pattern1.seq and Pattern1.wfm are created in the following location:

<Documents>\Keysight\PathWave\SignalGenerator\Waveforms

SCPI Command

[:SOURce]:RADio:PBUilding:WAVeform:GENerate

SCPI Example

RADio:PBUilding:WAVeform:GENerate

Couplings

 

Note

 

Preset

 

State Saved

Yes

Initial S/W Revision

A.18.00