Pulse Building

Pulse Width Types

Overview

The Pulse Width Type parameter allows you to apply patterns to the pulse width when the pulse type is trapezoidal or raised cosine. These patterns include: Linear Ramp, Staggered, and Stepped. A unique pulse width pattern can be applied to each pulse in the Pulse Building application.

The pulse width pattern is generated when you click the Generate button. The pattern generator will clip values that are out of range. A common example of this is when the pulse width pattern generator calculates a value that is greater than the current PRI. The pattern generator will return the smaller of the value calculated or the current PRI. The signal will be generated unless the target hardware does not have the required capabilities.

The current Pulse Builder Pattern property “Repeat” is used to specify the number of times to repeat the pulse on each line. For example, a Stepped width pattern can be selected, but if the number of Repeats is set to one (1), no pattern is generated. The exception to this is when the given pulse is use on multiple lines within a pattern. See the following example.

A given pulse may be used several times within a pulse pattern. When a given pulse is used throughout the pulse list, its pulse width pattern continues sequentially without reset.

Example:

In the following example, two pulses are used in the pattern. Pulse 1 has a "Stepped" pulse width pattern that increases from 10 us to 20 us using 11 steps of 1 us each. Pulse 2 has a constant pulse width of 5 us. Pulse 1 is repeated 8 times, Pulse 2 is repeated 4 times and finally Pulse 1 is repeated an additional 14 times.

The following figure shows the measured pulse widths generated by Pattern 1 where the stepped pulse width pattern continues and repeats after the fixed pulse width. Notice how the pulse width pattern for Pulse 1 continues without reset after Pulse 2.

When nesting patterns, the pulse width pattern continues when the pattern object is used on multiple lines within the new pattern. The pulse width pattern does not continue when the pattern object is used only once and the Repeat property is greater than one. In this case, the pulse width pattern created by the pattern object is repeated only the specified number of times.

Selecting the Pulse Width Type

Changing the Pulse Width Type resets some of the pulse width pattern properties. The actual width can be modified by the pulse width jitter value. Pulse width jitter is an impairment that can be used in addition to the pulse width pattern.

Setting Pulse Width Property Values

Pulse Width Start

This property is used by the Linear Ramp and Stepped pulse width patterns. Pulse Width Start also maps to the Width (100% - 100%) property.

Default

Min

Max

1 us/2 us

0

1 s

Pulse Width Stop

This property is used by the LinearRamp pulse width pattern. Changing the Pulse Width Pattern Type resets this property.

Default

Min

Max

5 us

0

1 s

Number of Pulses

This property is used by the Linear Ramp pulse width pattern. Changing the Pulse Width Pattern Type resets this property.

Default

Min

Max

5

1

10000

Pulse Width Step

This property is used only by the Stepped pulse width pattern. Changing the Pulse Width Pattern Type resets this property.

Default

Min

Max

1 us

–1 s

1 s

Number of Steps

This property is used by the Stepped pulse width pattern. The total pulses in the pattern equals Pulses Per Step x Number of Steps. Maximum pulse limit is hardware dependent. Changing the Pulse Width Pattern Type resets this property.

Default

Min

Max

4

1

10000

Pulses Per Step

This property is used by the Stepped pulse width pattern. The total pulses in the pattern equals Pulses Per Step x Number of Steps. The maximum pulse limit is hardware dependent. Changing the Pulse Width Pattern Type resets this property.

Default

Min

Max

1

1

10000

Staggered Pulse Width

The first width item in the list is mapped to the Width (100% - 100%) property such that changing the value of one property will change the value of the other. Changing the Pulse Width Pattern Type resets this property.

Default

Min

Max

1 array element

0

1 s