|
CALCulate:MEASure:CONVersion: |
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets or gets the parameter after conversion using the parameter conversion function, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<char> |
Select from the following of parameter after conversion:
|
|
Examples |
CALC:MEAS1:CONV:FUNC ZTSH |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:CONVersion:FUNCtion? |
|
Return Type |
Character |
|
"OFF" |
|
Last modified:
|
18-May-2016 |
First Release |