Controls format functions.
See Also
Example using this command.
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the display format for the measurement. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<char> |
Choose from: MLINear - Linear magnitude MLOGarithmic - Logarithmic magnitude PHASe UPHase - Unwrapped phase IMAGinary - Imaginary part (Im) REAL - Real part (Re) POLar - (Re, Im) SMITh SADMittance - Smith Admittance SWR - Standing Wave Ratio GDELay - Group Delay |
|
Examples |
CALC:MEAS:FORM MLIN |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FORMat? |
|
Return Type |
Character |
|
MLINear |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the units for the specified data format. Measurements with display formats other than those specified are not affected. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<dataFormat> |
Choose MLOG. |
|
<units> |
For unratioed measurements, choose from:
|
|
Examples |
CALC:MEAS:FORM MLOG, DBM |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:FORMat:UNIT? |
|
Return Type |
Character |
|
DBM |
|
Last modified:
|
18-May-2016 |
First Release |