|
CALCulate:MEASure:MIXer: |
Click on a Red keyword to view the command details.
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets or returns the swept parameter to display on the X-axis for the selected FCA measurement. Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<char> |
Parameter to display on the X-axis. Choose from: INPUT - Input frequency span OUTPUT - Output frequency span LO_1 - First LO frequency span LO_2 - Second LO frequency span |
|
Examples |
CALC:MEAS:MIX:XAX INPUT See an example that creates, selects, and calibrates an SMC measurement using SCPI. |
|
Query Syntax |
CALCulate<ch>:MEASure<mnum>:MIXer:XAXis? |
|
Return Type |
Character |
|
OUTPUT |
|
Last modified:
|
18-May-2016 |
First Release |