|
SENSe:COUPle: |
Click on a Red keyword to view the command details.
See Also
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON and OFF Time Domain Trace Coupling. All of the measurements in the specified channel are coupled.
Learn more about Time Domain Trace Coupling. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<bool> |
ON or 1 - Turns ON Time Domain Trace Coupling. OFF or 0 - Turns OFF Time Domain Trace Coupling. |
|
Examples |
SENS:COUP:PAR 0 |
|
Query Syntax |
SENSe<cnum>:COUPle:PARameter[:STATe]? |
|
Return Type |
Boolean |
|
ON or 1 |
|
Last Modified:
|
18-May-2016 |
First Release |