This VBScript program creates a new S21 measurement and displays it on the VNA screen.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as NewMeas.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
Dim app
Dim scpi
' Create / Get the VNA application.
Set app = CreateObject("AgilentPNA835x.Application")
Set scpi = app.ScpiStringParser
' A comment
'Preset the analyzer
scpi.Execute ("SYST:PREset")
'Define a measurement parameter
scpi.Execute ("CALCulate:MEASure1:PARameter 'S21'")