Perform Guided Mechanical Cal using SCPI


This sample programs perform a Guided Calibration using Mechanical standards for a 2-port cal (Ports 1 and 2).

Example in Excel VBA with VISA-COM

Sub SampleGuidedCal2Port()
   '*** The variables of the resource manager and the instrument I/O are declared.
   Dim ioMgr As VisaComLib.ResourceManager
   Dim GPIB As VisaComLib.FormattedIO488
   '*** The memory area of the resource manager and the instrument I/O are acquired.
   Set ioMgr = New VisaComLib.ResourceManager
   Set GPIB = New VisaComLib.FormattedIO488
   '*** Open the instrument.
   Set GPIB.IO = ioMgr.Open("GPIB0::16::INSTR")
   GPIB.IO.timeout = 10000

   Dim numSteps As Integer, strPrompt As String
   
   ' Specify the DUT connectors
   GPIB.WriteString "sens:corr:coll:guid:conn:port1 ""APC 3.5 female""", True

   GPIB.WriteString "sens:corr:coll:guid:conn:port2 ""APC 3.5 male""", True
   ' Note: If your PNA has more than 2 ports, you would need to uncomment
   ' one or both of these next two lines, to explicitly specify this is
   ' just a 2-port cal.
   'gpib.writestring "sens:corr:coll:guid:conn:port3 ""Not used"" ",True
   'gpib.writestring "sens:corr:coll:guid:conn:port4 ""Not used"" ",True
   MsgBox "Connectors defined for Ports 1 and 2"
   ' Select the Cal Kit for each port being calibrated.
   GPIB.WriteString "sens:corr:coll:guid:ckit:port1 ""85052D""", True
   GPIB.WriteString "sens:corr:coll:guid:ckit:port2 ""85052D""", True
   MsgBox "Cal kits defined for Ports 1 and 2"
   ' Initiate the calibration and query the number of steps
   GPIB.WriteString "sens:corr:coll:guid:init"
   GPIB.WriteString "sens:corr:coll:guid:steps?"
   numSteps = GPIB.ReadNumber
   MsgBox "Number of steps is " + CStr(numSteps)
   ' Measure the standards
   'The following series of commands shows that standards
   'can be measured in any order. These steps acquire
   'measurement of standards in reverse order.
   'It is easiest to iterate through standards using
   'a For-Next Loop.
   For i = numSteps To 1 Step -1
       step = "Step " + CStr(i) + " of " + CStr(numSteps)
       GPIB.WriteString "sens:corr:coll:guid:desc? " + CStr(i)
       strPrompt = GPIB.ReadString
       MsgBox strPrompt, vbOKOnly, step
       GPIB.WriteString "sens:corr:coll:guid:acq STAN" + CStr(i), True
   Next
   ' Conclude the calibration
   GPIB.WriteString "sens:corr:coll:guid:save", True
   MsgBox "Cal is done!"
   
   '*** End procedure
   GPIB.IO.Close
End Sub

Example in VB script

The following example is written in VB script.

The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.

This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as Guided.vbs. Learn how to setup and run the macro.

Dim app
Dim scpi

' Create / Get the VNA application.

Set app = CreateObject("AgilentPNA835x.Application")
Set scpi = app.ScpiStringParser

' Specify the DUT connectors

scpi.Execute "sens:corr:coll:guid:conn:port1 ""APC 3.5 female"" "
scpi.Execute "sens:corr:coll:guid:conn:port2 ""APC 3.5 male"" "

' Note: If your VNA has more than 2 ports, you would need to uncomment
' one or both of these next two lines, to explicitly specify this is
' just a 2-port cal.
'scpi.Execute "sens:corr:coll:guid:conn:port3 ""Not used"" "
'scpi.Execute "sens:corr:coll:guid:conn:port4 ""Not used"" "

MsgBox "Connectors defined for Ports 1 and 2"

' Select the Cal Kit for each port being calibrated.

scpi.Execute "sens:corr:coll:guid:ckit:port1 ""85052D"" "
scpi.Execute "sens:corr:coll:guid:ckit:port2 ""85052D"" "
MsgBox "Cal kits defined for Ports 1 and 2"

' Initiate the calibration and query the number of steps

scpi.Execute "sens:corr:coll:guid:init"
numSteps = scpi.Execute("sens:corr:coll:guid:steps?")
MsgBox "Number of steps is " + CStr(numSteps)

' Measure the standards
'The following series of commands shows that standards
'can be measured in any order. These steps acquire
'measurement of standards in reverse order.
'It is easiest to iterate through standards using
'a For-Next Loop.

For i = numSteps To 1
step = "Step " + CStr(i) + " of " + CStr(numSteps)
strPrompt = scpi.Execute("sens:corr:coll:guid:desc? " + CStr(i))
MsgBox strPrompt, vbOKOnly, step
scpi.Execute "sens:corr:coll:guid:acq STAN" + CStr(i)
Next

' Conclude the calibration

scpi.Execute "sens:corr:coll:guid:save"
MsgBox "Cal is done!"