The system power calibration is required after the configuration setup. After you installed all modules, the system power calibration should be executed once. The calibrated data is stored in your PC with your configuration. It is valid unless the configuration is changed. The purpose of calibration and procedure are different depending on the receiver module.
Purpose
Calibrate the source power level and linearity at the test ports.
Calibrate the source power for the parallel measurements.
Procedure
Calibration for power level only.
Purpose
Calibrate the source power level and linearity at the M9377A source output ports.
Procedure
Calibration for power level only.
Purpose
Calibrate the source power level and linearity at the test ports.
Acquire 1 port error term.
Procedure
Calibration for power level, S parameters and absolute measurement parameters.
In the procedure, one port is assigned as a reference port. The port is calibrated with a power sensor, then the other ports are calibrated with the reference port. If your configuration has any M9376As, the lowest number port of M9376A is assigned as the reference port. If your configuration has sets of M9377A and M9378A only, two ports are assigned as reference ports with the following priority (standard configuration, Wide Dynamic Range configuration, High Power configuration, High Gain configuration).
Note: Error Terms of cal set does not include the error terms of both M9377A and M9378A after user calibration.
Setting User Preset file is highly recommended when your configuration includes M9377A and M9378A modules. This can avoid occurring power unleveled error after every boot up.
Procedure
When you restart the firmware, set start frequency and initial power level properly. Then use the setting as “User preset status” from Preset > User Preset…, and select Save current state as User Preset and check User Preset Enable.
Typical setting for each configuration:
Configuration / Start frequency / Power
STD / 50 MHz / 0 dBm
DA / 50 MHz / 0 dBm
WDR / 500 MHz / -15 dBm
HP / 50 MHz / -30 dBm
HG / 500 MHz / -35 dBm
Required Equipment
|
|
Using Hardkey/SoftTab/Softkey |
When your configuration does not include any M9377As:
When your configuration includes M9377A:
Note: If the system power calibration is aborted, restart the Software Front Panel.
|
When the system power calibration and port configuration (for M9377A/78A) is not performed on the current configuration, the one of following messages is displayed at power on.
Set configuration using Port config wizard. Port config data is not found and typical data of DA config is used.
Port conifig data was found but corresponded system power cal file is not found. Typical system power cal data is used.
When the configuration is changed such as the module is replaced, this message will be displayed again and required to execute port configuration and system power calibration.
Last modified:
|
18-May-2016 |
New topic |