Performing Parameter Conversion of Measurement Results

Other 'Analyze Data' topics

Overview

You can use the parameter conversion function to convert the measurement results of the S-parameter (Sab) to the following parameters.

where:

Z0a: Characteristic impedance of port a

Z0b: Characteristic impedance of port b

When the fixture simulator function is ON and the port impedance function is ON, the value set in the port impedance conversion is used. In other cases, the system Z0 (preset value: 50 Ω) is used.

Selecting Conversion Target Parameter

  1. Press Meas > Meas Overview > Conversion

  2. Select function.

Softkey

Function

Off

Off

Z-Reflection

Impedance (Zr) in reflection measurement

Z-Transmit

Impedance (Zt) in transmission measurement

Z-Trans-Shunt

Impedance (Zt)  Transmission Shunt

Y-Reflection

Admittance (Yr) in reflection measurement

Y-Transmit

Admittance (Yt) in transmission measurement

Y-Trans-Shunt

Admittance (Yt) Transmission Shunt

1/S

Inverse S-paramete

Conjugation

Complex conjugate number