How to set Display Update |
|
Using Hardkey/SoftTab/Softkey |
|
Notes:
Turn ON/OFF the Display update will result on the Status Bar.
Update State ON/OFF is part of the save/recall state.
Softkey(s) exist for update state ON/OFF and immediate update.
Disable the display update will yield the most significant performance improvements. The performance improvement (due to disabling updates) for a single channel and window state seems negligible. However, with a large number of channels, windows and traces, it should make more of a difference (but disabling the display update will provide more performance improvement). For example, Performance Oddities, the following is looking at the INDEX line (Handler I/O) for a 1.0GHz to 1.2GHz with 201 point sweep (otherwise Preset condition apply). When high, the box is sweeping. There is 20ms of dead time between many of sweeps.
Last modified:
|
18-May-2016 |
First Release |