Click on image areas to learn more.
The VNA display is controlled by a third-party display driver. This driver is capable of producing many display effects which are beyond the basic needs of the VNA measurement environment. Keysight does not specify or warranty these display settings.
WARNING: The VNA display must remain in the 16-bit color setting in order to comply with international emissions regulations.
When using external programs to control the VNA, it is possible that the display settings may become corrupt. When this occurs, the following will restore the VNA display settings:
Press System > Main > Minimize Application.
Right-click on the desktop, then click Personalize.
On the Themes tab, select Keysight Theme.
Front Panel Tour
Learn to test the display screen
The VNA is equipped with a 12.1-inch High resolution, color, touch-sensitive LCD screen for displaying traces, softkeys, and other measurement related information. The touchscreen LCD allows you to make measurement settings by touching the LCD screen directly with a finger.
|
Important:
|
How to Calibrate or turn ON | OFF the Touchscreen |
|
Using Hardkey/SoftTab/Softkey |
|
|
The touchscreen ON | OFF setting remains until changed again from this menu, the Preferences dialog, or remotely. |
Allows you easily select the tools. Learn more.
Provides details of each trace in the window. Highlighted trace indicates the active trace. Learn more.
Along with the softkeys, allows numeric values to be entered for settings.
Provides stimulus and response information for markers. Learn about Customizing the Marker Readout Area. See also Marker Drag.
The combination of hardkeys and softkeys allow easy access to all VNA features without a mouse.
These indicates that pressing the tabs will display softkeys.
Performs interface operations that are equivalent to those of keys in the INSTRUMENT keys, RESPONSE keys, STIMULUS keys and UTILITY keys on the front panel of VNA. Learn more.
Provides window identification which is useful for remote programmers.
Provides detail about all aspects of the status of the VNA. Learn more.
Displays the start and stop values of the sweep range.
These is known as shortcut icon in order to allows you to quickly select the tools on softkey. Learn more.
Drag a displayed marker across the trace using a finger (with touchscreen ON) or a mouse. Learn more.
Cursor changes to a “hand” when hovering over a clickable object.
Right-click on the Entry toolbar to launch a mouse-compatible numeric pad.
Right-click on a window area to make selections pertaining to that window.
Double-click on a window area to maximize the window. To return to original window configuration, right-click on window area, then click Tile.
Left-click on X-axis annotation to select the active channel/trace.
Right-click on X-axis annotation and click Start/Stop/Center... to change stimulus properties.
Quickly change Scale, Reference Level, and Position. Learn how.
Right-click on Y-axis annotation and click Scale... to change Scale.
Drag a trace from one window to another. Click or touch either the trace or the Trace Status. Drag the trace to another window, then release the mouse or lift your finger.
Left-click a trace or Trace Status to make it the selected trace.
Double-click on a trace or Trace Status to maximize the trace. Double-click again to return to the original trace configuration. See programming commands.
Set a preference to always widen the active trace.
Set a preference to briefly widen the active trace.
Drag a trace from one window to another. Click or touch either the trace or Trace Status. Drag the trace to another window, then release the mouse or lift your finger.
Right-click on a trace or Trace Status to add a marker.
Right-click a marker to make selections pertaining to that marker, such as Marker Search or Function.
Use the Touchscreen or adjacent buttons to select from eight dynamic softkey menu choices.
To Show the softkeys, press any front-panel hardkeys on the screen that launches a softkey menu.
|
Item |
Description |
|
|
Selection launches a dialog box. |
|
|
Selection launches more related softkeys on the left side. |
Last Modified:
|
18-May-2016 |
First Release |