Downloading and Extracting Waveform Data

You can download I/Q data, marker files, or encrypted files into the PXB file system. For information on waveform structure, see Understanding Encrypted Waveform Structure.

You can download or extract waveform data created in any of the following ways:

Transferring Signal Studio Waveforms

When you download a waveform using an Agilent Signal Studio software product, you can use Windows file sharing, or SCPI commands to transfer the file to the PXB using one of the following protocols:

Downloading Waveform Data Using SCPI Commands

You can download waveform data using the following SCPI commands:

:MMEMory:DATA "<file_name>",<data_block>

The PXB expects to see waveform data as block data (binary files). The IEEE standard 488.2-1992 section 7.7.6 defines block data. The following example shows how to structure a SCPI command for downloading waveform data (#ABC represents the block data):

:MMEM:DATA "<file_name>",#ABC

"<file_name>"

the I/Q file name and file path within the PXB

#

indicates the start of the data block

A

the number of decimal digits present in B

B

a decimal number specifying the number of data bytes to follow in C

C

the actual binary waveform data

 

There are 3 ways to specify a "<file_name>":

  1. Specify the file name "<myFile>” that will store the file in D:\User_My_Documents. 

  1. Specify the file name with the full path "<D:\my_folder\myFile>” that will store the file in D:\my_folder\myFile .

  2. Use the non-volatile file name: "NVWFM[1,2,3,...9]:my waveform.bin)". The file will be stored in the respective directory: D:\Waveforms\Channel[1,2,3,...9].

The following example demonstrates this structure:

 

NVWFM1:

the file path

my_file

the I/Q file name as it will appear in the PXB’s memory catalog

#

indicates the start of the data block

3

B has three decimal digits

240

240 bytes of data to follow in C

12%S!4&07#8g*Y9@7...

the ASCII representation of some of the binary data downloaded to the PXB, however not all ASCII values are printable.