The two tabs shown below access the Master Setup parameters for adding real-time fading to custom or Signal Studio generated waveforms. Additionally, clicking the Fader block in the block configuration or Fader Path node in the tree view displays the Fader Path parameters for the selected Fader Channel model.
|
|
Run-time Adjustment of Fading Parameters For 1 Channel Generate and Fade or 1 Channel Fade (ext in) configurations:
|
Click a tab to display information for the related parameter settings.
Applying the Restore Default Settings button in the Fader Setup view restores the default settings for the carrier frequency and the random seed and all Fader Paths to their default settings for the selected channel model.
Displays the channel bandwidth depending on the number of enabled paths.
Configurations with regular channels:
| Paths | Standard | R2C License (U01 or later) |
|---|---|---|
| 0-6 | 120 MHz | 160 MHz |
| 7-12 | 80 MHz | 80 MHz |
| 13-24 | 40 MHz | 40 MHz |
Configurations with split channels that require split fading Option N5106A-169 (e.g., 2x8 MIMO and 4x4 MIMO):
| Paths | Standard | R2C License (U01 or later) |
|---|---|---|
| 0-6 | 60 MHz | 80 MHz |
| 7-12 | 40 MHz | 40 MHz |
| 13-24 | 20 MHz | 20 MHz |
Using data from an external source, you can configure up to four independent fading channels in one of several ways:
select a standard model for the fader that automatically populates the path configurations as defined by the respective standard committee.
manually define channel correlation if all paths have the same settings, non-zero Doppler frequency, and use Rayleigh fading (not Jakes).
enter user-defined path data to more closely simulate the real-world environment of your DUT.
|
gives information on setting general fading parameters, available standard models and associated profiles. |
|
|
displays the correlation coefficients according to the current channel configuration. |
|
|
defines the parameters for the fading paths. |