Corrections/De-embedding

This capability requires license model E7653APPC.

This topic describes the RF Output > Corrections/De-embedding screen, where you can configure and apply external corrections for your test setup.

Overview

Corrections On

Center Frequency Corrections Only

Add from Measurement

Configure Sensor ClosedSetup

Power Measurement Device

Start Frequency

Stop Frequency

Number of Steps

Power Meter Properties ClosedSetup

Power Meter Connection Type

Power Meter IP Address

Power Meter HiSLIP Device Name

Power Meter USB Device Name

Power Meter USB Device Name List

Power Meter IP Port

Power Meter Channel from the Device List

Power Meter Calibrate Sensor

Power Meter Calibrate Sensor from the Device List

Power Meter Zero Sensor

Power Meter Zero Sensor from the Device List

Spectrum Analyzer Properties ClosedSetup

Spectrum Analyzer Connection Type

Spectrum Analyzer Hostname or IP Address

Spectrum Analyzer HiSlip Address

Spectrum Analyzer USB Device Name

Spectrum Analyzer IP Port

Spectrum Analyzer USB Device Name List

Measure Correction Data

Abort

Block Properties ClosedSetup

Count

Add Fixture

Clear

Delete Block

Move Left or Move Right

Enable

File

De-embed/embed

Reverse Ports

Snn = 0

Characterize ClosedSetup

Start Frequency

Stop Frequency

Number of Points

Power (Total RMS)

IF Bandwidth

ECal USB Device Name List

ECal USB Device

ECal Port

ECal Compression Level

ECal Damage Level

Run Measurement

Abort

Absolute Power Table Preset

Absolute Power Table Pair

Absolute Power Table Points

Absolute Power Table Frequency

Absolute Power Table Store

Absolute Power Table Initialize Frequency Step

DUT Reflection Coefficient ClosedSetup

Overview

File

Enable

Center Frequency Corrections Only

Delta

Add from Measurement ClosedSetup

Run Measurement

Abort

Measurement Start Frequency

Measurement Stop Frequency

Measurement Number of Points

Measurement IF Bandwidth

Overview

The instrument has the capability to extend the Reference Plane beyond the factory calibrated RF Output port. The Reference Plane can be extended via Corrections and/or S-parameter de-embedding.

Up to four stages of correction and de-embedding are available. These stages are referred to as blocks and are labeled as Block A, B, C, and D. For SCPI commands, block A=1, B=2, and so on.

The following table lists the available correction and de-embedding components for your test setup.

Component Purpose Supported File Format(s)
Factory Cal

Directly measured correction data created during the factory manufacturing process or annual calibration.

N/A
Block A

User correction data applied on top of the Factory Cal.

For this block, you can:

  • either apply corrections from a specified correction file.

  • or measure directly with a supported power meter, spectrum analyzer, or network analyzer to generate a correction file.

.csv

.uflat (for compatibility with other Keysight Technologies signal generators)

Block B

De-embedding of fixtures including cables, connectors, and other passive components between the instrument and DUT to remove the effects of these test fixtures from the measurement results.

Individual fixture blocks represent different fixture elements in your test setup.

Calculated correction data for the sum of Blocks B, C, and/or D is applied on top of the Block A and/or Factory Cal.

Prior to the software version A.14.00, only the S21 data of the fixture was used for correction. With software version A.14.00 or later, the S11 and S21 data of the fixture are used for correction. Due to this difference in the S-parameters used for correction in these software versions, the calculated correction data may vary for these software versions.

To apply corrections for a fixture, you can:

  • either use an existing .s2p correction file.

  • or generate a .s2p correction file for the fixture using an ECal device. Requires Option V08.

.s2p
Block C
Block D
DUT

Compensation for the instrument to DUT mismatch.

For this block, you can:

  • either apply corrections from a specified correction file.

  • or measure directly to generate a correction file.

Requires Option V08.

See DUT Reflection Coefficient.

.s1p

Configuring and applying user correction data using Block A

Adding fixture blocks (Block B, C, or D) for de-embedding/characterization

Corrections On

Enables or disables the user-flatness corrections.

GUI Location

RF Output > Corrections/De-embedding > Corrections On

SCPI Command

[:SOURce][:RF<channel>]:CORRection[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection[:STATe]?

SCPI Example

CORR ON

CORR?

Notes Output power may become too high when Corrections/Deembedding fixture's S-parameter includes S21 = 0.

Preset

0

State Saved

Yes

Backwards Compatibility SCPI

N51XXB:

[:SOURce]:CORRection[:STATe]

Backwards Compatibility Notes

For N51xxB:

Expand [:SOURce]:CORRection[:STATe] to [:SOURce][:RF<channel>]:CORRection[:STATe]

Center Frequency Corrections Only

Ignores the complex response data in measured (block A) or s2p (block B, C, D) data and only applies the absolute power, phase and time corrections.

GUI Location

RF Output > Corrections/De-embedding > Center Frequency Correction Only

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CFConly[1]|2[:STATe] ON|OFF|0|1

[:SOURce][:RF<channel>]:CORRection:CFConly[1]|2[:STATe]?

SCPI Example

For Block A:

CORR:CFC ON

CORR:CFC?

For Block B, C, D

CORR:CFC2 ON

CORR:CFC2?

Preset

0

State Saved

Yes

Backwards Compatibility SCPI

[:SOURce][:RF<channel>]:CORRection:APConly[:STATe]

Backwards Compatibility Notes

Alias [:SOURce][:RF<channel>]:CORRection:APConly[:STATe] to

[:SOURce][:RF<channel>]:CORRection:CFConly[1][:STATe];

[:SOURce][:RF<channel>]:CORRection:CFConly2[:STATe]

See Also - DUT Reflection Coefficient > Center Frequency Corrections Only

Add from Measurement

You can use the Block A properties > Add from Measurement button to access the Measure Corrections wizard. Using this wizard, you can configure and run the user correction measurement. The correction data generated from this measurement is saved to a .csv file. This file is then used as the correction file.

The subsections below describe the SCPI commands available to configure and run the user correction measurement.

Configure Sensor

SCPI commands defined in this section can be used to set up Correction measurements and Power Sensors used. In the user interface, these settings are included in the RF Output block's, Corrections/De-embedding block setup, when the Add from Measurement button is selected.

Supported measurement devices are as follows.

Keysight U8480 Series USB Thermocouple Power Sensor

Keysight U2000 Series USB Sensors

Including:

U2000 Series USB Power Sensors:

X-Series Signal Analyzers:

Use Device List

Enables the Device List to be the sole method of specifying a Spectrum Analyzer or Power Meter to be used for Correction Measurement.

To configure external devices in the Device List, see Device List.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure Sensor > Power Measurement Device > Use Device List (checkbox)

SCPI Command

[:SOURce][:RF<channel>]:CORRection:DLISt ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:DLISt?

SCPI Example

RF3:CORR:DLIS ON

RF3:CORR:DLIS?

Preset

This is unaffected by a Preset but is set to OFF on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Choices

ON | OFF | 1 | 0

Specify Device for Correction Measurement

Specifies a Power Meter or a Spectrum Analyzer from the Device List for user Correction Measurement. Note that the reference clock must be locked between the signal generator and Spectrum Analyzers.

To configure external devices in the Device List, see Device List.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure Sensor > Power Measurement Device > Use Device List (selected) > Configure Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:DEVice <name>

[:SOURce][:RF<channel>]:CORRection:DEVice?

SCPI Example

RF3:CORR:DEV "myDevice"

RF3:CORR:DEV?

Notes

If the specified device does not exist in the Device List, an error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Spectrum Analyzer or Power Meter, an error will be raised:

-220,"Parameter error; Correction Measurement requires a Spectrum Analyzer or Power Meter device type"

Couplings

If the device currently selected from the Device List is removed, this setting will default to NONE

Value will only be utilized by hardware when Use Device List for Correction Measurement is set to ON.

Preset

This is unaffected by a Preset but is set to an empty string on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Power Measurement Device

Selects the hardware type used in the user correction measurement when the Device List is not being used.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure Sensor > Power Measurement Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMDevice PMETer|SANalyzer

[:SOURce][:RF<channel>]:CORRection:PMDevice?

SCPI Example

CORR:PMD PMET

CORR:PMD?

Couplings

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

PMETer

State Saved

Yes

Choices

Power Meter | Spectrum Analyzer

Start Frequency

Sets the start frequency for the corrections calibration step array.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Start Frequency

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STARt <freq>

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STARt?

SCPI Example

CORR:FLAT:STEP:STAR 1GHz

CORR:FLAT:STEP:STAR?

Couplings

Coupled to Stop Frequency. If Start Frequency goes above Stop Frequency, Stop Frequency is automatically adjusted to Start Frequency.

Preset

1 GHz

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: Max

State Saved

Yes

Min

9 kHz

Max

For N5185A/N5186A:

  • With Option 503: 3 GHz

  • With Option 506: 6 GHz

  • With Option 508: 8.5 GHz

Resolution

0. 00001 Hz

Stop Frequency

Sets the stop frequency for the corrections calibration step array.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Stop Frequency

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STOP <freq>

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:STOP?

SCPI Example

CORR:FLAT:STEP:STOP 1GHz

CORR:FLAT:STEP:STOP?

Couplings

Coupled to Start Frequency. If Stop Frequency goes below Start Frequency, Start Frequency is automatically adjusted to Stop Frequency.

Preset

2 GHz

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: Max

State Saved

Yes

Min

9 kHz

Max

For N5185A/N5186A:

  • With Option 503: 3 GHz

  • With Option 506: 6 GHz

  • With Option 508: 8.5 GHz

Resolution

0.00001 Hz

Number of Steps

Defines the number of points in the corrections calibration step array.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Number of Steps

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP:POINts <integer>

[:SOURce][:RF<channel>]:CORRection:FLATness:STEP: POINts?

SCPI Example

CORR:FLAT:STEP:POIN 2

CORR:FLAT:STEP:POIN?

Preset

10

When SCPI Backward Compatibility Mode is N51xxB:

  • For Channel 1: 2

State Saved

Yes

Min

2

Max

10000

Power Meter Properties

Sets the power meter properties when Power Meter is the selected Power Measurement Device.

Power Meter Connection Type

Sets the type of control connection for communication using the external power meter for corrections calibration.

HISLip

Enables the power meter for HiSlip control through the signal generator

SOCKets

Enables the power meter for sockets LAN control through the signal generator.

USB

Enables the power meter for USB control through the signal generator.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN, HiSLIP, Socket) or USB

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:TYPE SOCKets|USB|HISLip

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:TYPE?

SCPI Example

CORR:PMET:COMM:TYPE SOCK

CORR:PMET:COMM:TYPE?

Notes

The settings enabled by this command are not affected by a signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

VXI11 is not available on N5185A and N5186A, attempting to set VXI11 raises Invalid Parameter error.

Preset

SOCKets

State Saved

No

Choices

Socket | USB | HiSlip

Power Meter IP Address

Sets the internet protocol (IP) address for a power meter that is controlled by the signal generator for corrections calibration. If connecting to a GPIB power meter through a LAN-GPIB gateway, this command sets the IP address of the gateway.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > Connection Type LAN > Set LAN IP Address

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:IP <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:IP?

SCPI Example

CORR:PMET:COMM:LAN:IP "192.168.1.5"

CORR:PMET:COMM:LAN:IP?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST. Ensure that the power meter IP address is different from the signal generator address.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Power Meter HiSLIP Device Name

Specifies the HiSLIP device name for a power meter that is being controlled by the signal generator for corrections calibration. If connecting directly to the power meter, enter the name as specified in your power meter documentation.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type LAN > HiSLIP > Remote Name

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:HISLip:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:HISLip:DEVice?

SCPI Example

CORR:PMET:COMM:HISL:DEV "hslip1"

CORR:PMET:COMM:HISL:DEV?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

hislip0

State Saved

No

Power Meter USB Device Name

Selects the USB device to be used for corrections calibration. The query returns the USB device identification.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type USB > Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:USB:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:USB:DEVice?

SCPI Example

CORR:PMET:COMM:USB:DEV "instr0"

CORR:PMET:COMM:USB:DEV?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Power Meter USB Device Name List

Remote command only.

Returns a listing of all connected USB devices.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:USB:LIST?

SCPI Example

CORR:PMET:COMM:USB:LIST?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

State Saved

No

Power Meter IP Port

Sets the IP port number on the power meter that is controlled by the signal generator for corrections calibration.

5025

Standard mode. The command enables standard mode for simple programming.

5024

Telnet mode. The command enables the telnet SCPI service for programming.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type LAN > Protocol set to Socket > Port Number

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:PORT <integer>

[:SOURce][:RF<channel>]:CORRection:PMETer:COMMunicate:LAN:PORT?

SCPI Example

CORR:PMET:COMM:LAN:PORT 5025

CORR:PMET:COMM:LAN:PORT?

Notes

The settings enabled by this command are not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

5025

State Saved

No

Power Meter Channel from the Device List

Selects the channel setting on the external power meter used for calibration from the Device List.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Use Device List (checked) > Configure Device > (select or add a device) > Power Meter Channel (drop-down menu)

Preset

This is unaffected by a Preset but is set to A on a "Restore System Settings to Default Values."

Range

Channel 1 | Channel 2 | Channel 3 | Channel 4

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Power Meter Calibrate Sensor

Calibrates the connected power meter. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Calibrate Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:CALibrate

SCPI Example

CORR:PMET:CAL

Power Meter Calibrate Sensor from the Device List

Calibrates the connected power meter from the Device List. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Use Device List (checked) > Configure Device > (select or add a device) > Calibrate Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:CALibrate:DLISt <string>

SCPI Example

CORR:PMET:CAL:DLIS "myDevice"

Notes

If the specified device does not exist in the Device List, an error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Power Meter, an error will be raised:

-220,"Parameter error; Power Meter Calibrate Sensor requires a Power Meter device type"

Power Meter Zero Sensor

Zeroes the connected power meter. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Zero Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:ZERO

SCPI Example

CORR:PMET:ZERO

Power Meter Zero Sensor from the Device List

Zeroes the connected power meter from the Device List. This is an immediate action.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Next > Use Device List (checked) > Configure Device > (select or add a device) > Zero Sensor

SCPI Command

[:SOURce][:RF<channel>]:CORRection:PMETer:ZERO:DLISt <string>

SCPI Example

CORR:PMET:ZERO:DLIS "myDevice"

Notes

If the specified device does not exist in the Device List, an error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Power Meter, an error will be raised:

-220,"Parameter error; Power Meter Zero Sensor requires a Power Meter device type"

Spectrum Analyzer Properties

Sets the spectrum analyzer properties when Spectrum Analyzer is the selected Power Measurement Device.

Spectrum Analyzer Connection Type

Sets the type of control connection for communication with the external spectrum analyzer for corrections calibration.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN, HiSLIP, Socket) or USB

HISLip

Enables the spectrum analyzer for HiSlip control through the signal generator.

SOCKets

Enables the spectrum analyzer for sockets LAN control through the signal generator.

USB

Enables the spectrum analyzer for USB control through the signal generator.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:TYPE SOCKets |USB|HISLip

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:TYPE?

SCPI Example

CORR:SAN:COMM:TYPE SOCK

CORR:SAN:COMM:TYPE?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

SOCKets

State Saved

No

Choices

Socket | USB | HiSlip

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:TYPE

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:TYPE to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:TYPE

Spectrum Analyzer Hostname or IP Address

Sets the internet protocol (IP) address for a spectrum analyzer that is controlled by the signal generator for corrections calibration. If connecting to a GPIB spectrum analyzer through a LAN-GPIB gateway, this command sets the IP address of the gateway.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > Hostname or IP Address

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:IP <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:IP?

SCPI Example

CORR:SAN:COMM:LAN:IP "192.168.1.5"

CORR:SAN:COMM:LAN:IP?

Notes

  • The setting enabled by this command is not affected by signal generator power-on, preset, or *RST. Ensure that the spectrum analyzer IP address is different from the signal generator address.

  • Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:LAN:IP

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:LAN:IP to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:LAN:IP

Spectrum Analyzer HiSlip Address

Enter a HiSlip device name for a spectrum analyzer that is being controlled by the signal generator for corrections calibration. If connecting directly to the spectrum analyzer, enter the name as specified on your spectrum analyzer documentation.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > HiSLIP > Address

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:HISLip:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:HISLip:DEVice?

SCPI Example

CORR:SAN:COMM:HISL:DEV "instr0"

CORR:SAN:COMM:HISL:DEV?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

hislip0

State Saved

No

Spectrum Analyzer USB Device Name

Selects the USB device to be used for corrections calibration. The query returns the USB device identification.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > USB > Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:USB:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:USB:DEVice?

SCPI Example

CORR:SAN:COMM:USB:DEV "instr0"

CORR:SAN:COMM:USB:DEV?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

State Saved

No

Spectrum Analyzer IP Port

Sets the spectrum analyzer's IP port number that is controlled by the signal generator for corrections calibration.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Configure > Connection Type > LAN > Protocol set to Socket > Port

5025

Standard mode. The command enables standard mode for simple programming.

5024

Telnet mode. The command enables the telnet SCPI service for programming.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:PORT <integer>

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:LAN:PORT?

SCPI Example

CORR:SAN:COMM:LAN:PORT 5025

CORR:SAN:COMM:LAN:PORT?

Notes

  • The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

  • Value will only be utilized by the instrument when Use Device List for Correction Measurement is set to OFF.

Preset

5025

State Saved

No

Backwards Compatibility SCPI

N51xxB:

:SYSTem:SANalyzer:COMMunicate:LAN:PORT

Backwards Compatibility Notes

For N51xxB:

Alias :SYSTem:SANalyzer:COMMunicate:LAN:PORT to [:SOURce][:RF1]:CORRection:SANalyzer:COMMunicate:LAN:PORT

Spectrum Analyzer USB Device Name List

Remote command only.

Query only. Returns a listing of all connected USB devices.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:SANalyzer:COMMunicate:USB:LIST?

SCPI Example

CORR:SAN:COMM:USB:LIST?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

State Saved

No

Measure Correction Data

The measured correction data will be saved to the specified file. The file path can be either a full or a relative path. When a relative path is given as file path, it will be based from:

Corrections

If no file is specified, a file name is automatically created.

This is an overlapped command that initiates the Correction Data measurement. The measurement can be aborted by the Abort command.

Note that the reference clock must be locked between the signal generator and the spectrum analyzer.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Measure Corrections > Measure Correction Data

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:CALibrate [<file_name>]

SCPI Example

CORR:FLAT:CAL

State Saved

No

Abort

Aborts the Correction Data measurement.

GUI Location

RF Output > Corrections/De-embedding > Add from Measurement > Measure Corrections > Abort

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:CALibrate:ABORt

SCPI Example

CORR:FLAT:CAL:ABOR

State Saved

No

Block Properties

There can be up to four blocks in Corrections Setup. These blocks belong to the following two types.

To access Block Properties from the GUI, click on the applicable Block- Block A, Block B, Block C or Block D.

Count

Displays or returns the number of Blocks configured for corrections. The maximum number of blocks is four. The minimum number is 1. The first block is for User Corrections and is always present.

GUI Location

RF Output > Corrections/De-embedding

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk:COUNt?

SCPI Example

CORR:BLOC:COUN?

Add Fixture

Adds a fixture block at the end of blocks.

GUI Location

RF Output > Corrections/De-embedding > Add Fixture

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk:ADD:FIXTure [<file_name>[,<apply>[,<rport>]]]

SCPI Example

CORR:BLOC:ADD:FIXT "data.s2p"

Notes

For instruments with Option V08:

  • Optional variables <file_name>, <apply>, and <rport> can be omitted as Option V08 allows you to generate a .s2p file for the fixture using an ECal device and use this file as the fixture characterization correction file.

For instruments without Option V08:

  • Attempting to send a SCPI without <file_name> raises the error -109, "Missing parameter". <apply> and <rport> can be omitted.

State Saved

No

Clear

Remote command only.

Clears all the blocks except for the first one. The first block is for User Correction and cannot be deleted from the list.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk:CLEar:FIXTure

SCPI Example

CORR:BLOC:CLE:FIXT

Delete Block

Deletes the specified block. If the specified block doesn’t exist, it issues an error.

There is no SCPI command for this function.

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Delete Block

Move Left or Move Right

Moves the specified block to the specified position. If the specified block doesn’t exist, it issues an error. If the destination block is smaller than the number of blocks, it issues an error.

There is no SCPI command for this function.

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Move Left or Move Right

File

Sets or queries the correction data file (.csv or .uflat) for Block A and .s2p file for Block B, C, or D.

The default folder location is:

For N5185A and N5186A:

Top level of filesystem\Corrections

File format for Block A

For Block A (1 in SCPI), the file can be a .uflat file compatible with other Keysight Technologies signal generators, or a .csv file.

The .csv file must be formatted as follows:

<Frequency in Hz>,<Amplitude in dB>,<Phase in radian>

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Change File, current file name

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk[1]|2|3|4:FILE <file_name>

[:SOURce][:RF<channel>]:CORRection:BLOCk[1]|2|3|4:FILE?

SCPI Example

CORR:BLOC:FILE "FixtureChannel2"

Notes

Attempting to load a Block A .csv file with four elements in a row, without N7653APPC of subscription date of June 1, 2024 or later, raises the error +703, Feature not supported; N7653APPC with subscription date June 1, 2024, is required.

Attempting to load a Block A .csv file with four elements in a row, on an unsupported instrument will raise the error +703, Feature not supported; Correction file cannot contain four elements on {Model}.

Preset

""

State Saved

Yes

Backwards Compatibility SCPI

N51xxB:

[:SOURce]:CORRection:FLATness:LOAD

Backwards Compatibility Notes

For N51xxB:

  • Alias [:SOURce]:CORRection:FLATness:LOAD to [:SOURce]:RF1:CORRection:BLOCk1:FILE

  • .userflat is appended to the filename.

  • Alias [:SOURce][:RF<channel>]:CORRection:FLATness:LOAD to [:SOURce][:RF<channel>]:CORRection:BLOCk1:FILE

  • The aliased command applies to Block 1/A only.

Enable

Enables or disables the selected block.

GUI Location

RF Output > Corrections/De-embedding > select applicable Block > Block Properties > Enable

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk{1:4}[:STATe] ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:BLOCk{1:4}[:STATe]?

SCPI Example

CORR:BLOC 1

CORR:BLOC?

State Saved

Yes

De-embed/embed

Specifies how the data is applied to the cascaded correction data. When De-embed is selected, the output at the frequency point is adjusted to compensate for the amplitude and phase changes introduced by the block. When Embed is selected, it is adjusted to include them.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Deembed or Embed

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:APPLy DEEMbedding|EMBedding
[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:APPLy?

SCPI Example

CORR:BLOC2:APPL EMB

CORR:BLOC2:APPL?

State Saved

Yes

Choices

De-embed | Embed

Reverse Ports

Specifies whether the port is reversed or not.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Reverse Ports

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:RPORt ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:BLOCk{2:4}:RPORt?

SCPI Example

CORR:BLOC2:RPOR 1

CORR:BLOC2:RPOR?

State Saved

Yes

Snn = 0

Enables or disables Snn = 0.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Snn = 0

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk2|3|4:REFLection:ZERO ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:BLOCk2|3|4:REFLection:ZERO?

SCPI Example

CORR:BLOC2:REFL:ZERO 1

CORR:BLOC2:REFL:ZERO?

Preset OFF

State Saved

Yes

Characterize

Requires Option V08

Click the Characterize button to access the Fixture Characterization screen. You can use Fixture Characterization to generate a .s2p file for a fixture using an ECal USB device and use this file as the fixture characterization correction file.

Supported ECal devices for fixture characterization

Fixture Characterization can be measured on all channel configurations (single, dual, or quad).

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize

The settings shown in the following screen are available for configuring Fixture Characterization correction file.

Start Frequency

Sets the start frequency for the Fixture Characterization Measurement correction point array. This setting is shared among all blocks.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > Start Frequency

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:STARt <freq>

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:STARt?

SCPI Example

RF1:CORR:FIXT:CHAR:STAR 3GHz

RF1:CORR:FIXT:CHAR:STAR?

Coupling Coupled to Stop Frequency. If Start Frequency goes above Stop Frequency, Stop Frequency is automatically adjusted to Start Frequency.

Preset

10 MHz

State Saved

Yes

Min

9 kHz

Max

With option 503 = 3 GHz

With option 506 = 6 GHz

With option 508 = 8.5 GHz

Resolution 0.00001 Hz

Stop Frequency

Sets the stop frequency for the Fixture Characterization Measurement correction point array. This setting is shared among all blocks.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > Stop Frequency

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:STOP <freq>

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:STOP?

SCPI Example

RF1:CORR:FIXT:CHAR:STOP 3GHz

RF1:CORR:FIXT:CHAR:STOP?

Coupling Coupled to Start Frequency. If Stop Frequency goes below Start Frequency, Start Frequency is automatically adjusted to Stop Frequency.

Preset

8 GHz

State Saved

Yes

Min

9 kHz

Max

With option 503 = 3 GHz

With option 506 = 6 GHz

With option 508 = 8.5 GHz

Resolution 0.00001 Hz

Number of Points

Sets the number of points in the Fixture Characterization Measurement correction step array. A frequency spacing of 10 MHz is optimal. This setting is shared among all blocks.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > Number of Points

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:POINts <integer>

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:POINts?

SCPI Example

RF1:CORR:FIXT:CHAR:POIN 1000

RF1:CORR:FIXT:CHAR:POIN?

Preset

201

State Saved

Yes

Min 2
Max

8500

Power (Total RMS)

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > Power (Total RMS)

SCPI Command

Refer to Power (Total RMS)

IF Bandwidth

Sets the IF bandwidth for the Fixture Characterization Measurement. Reducing the IF receiver bandwidth reduces the effect of random noise on a measurement. Each tenfold reduction in IF bandwidth lowers the noise floor by 10 dB. This setting is shared among all blocks.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > IF Bandwidth

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:BANDwidth <freq>

[:SOURce][:RF<channel>]:CORRection:FIXTure:CHARacterize:BANDwidth?

SCPI Example

RF1:CORR:FIXT:CHAR:BAND 100

RF1:CORR:FIXT:CHAR:BAND?

Preset

1 kHz

State Saved

Yes

Min 1 Hz
Max

100 MHz

Resolution 1 Hz

ECal USB Device Name List

Query only. Returns a list of all connected USB devices.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CKIT:COMMunicate:USB:LIST?

SCPI Example

CORR:CKIT:COMM:USB:LIST?

Notes

The setting enabled by this command is not affected by signal generator power-on, preset, or *RST.

State Saved

No

ECal USB Device

Specifies the ECal device to use by name for the fixture characterization. The .s2p file for the fixture is generated using the specified ECal device.

See Supported ECal devices for fixture characterization

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > ECal USB Device

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CKIT:COMMunicate:USB:DEVice <string>

[:SOURce][:RF<channel>]:CORRection:CKIT:COMMunicate:USB:DEVice?

SCPI Example

CORR:CKIT:COMM:USB:DEV "instr0"

CORR:CKIT:COMM:USB:DEV?

Preset This is unaffected by a Preset but is set to an empty string on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

ECal Port

Specifies the ECal port to be used for fixture characterization.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > ECal port

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CKIT:PORT A|B|C|D

[:SOURce][:RF<channel>]:CORRection:CKIT:PORT?

SCPI Example

CORR:CKIT:PORT A

CORR:CKIT:PORT?

Preset This is unaffected by a Preset but is set to A on a "Restore System Settings to Default Values."
Range A|B|C|D

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

ECal Compression Level

Remote Command - Query only.

Returns the compression level for the connected ECal device.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CKIT:POWer:COMPression?

SCPI Example

CORR:CKIT:POW:COMP?

Notes When the connected ECal device is not supported, or no ECal device is connected, this command returns 999 dBm.

ECal Damage Level

Remote Command - Query only.

Returns the damage level for the connected ECal device.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CKIT:POWer:DAMage?

SCPI Example

CORR:CKIT:POW:DAM?

Notes When the connected ECal device is not supported, or no ECal device is connected, this command returns 999 dBm.

Run Measurement

Runs the Fixture Characterization Measurement.

The Fixture Characterization Measurement can be aborted using the Abort command.

Upon successful completion of the measurement:

Additionally, you can also include user data in the resulting .s2p file’s header when specified via the Run Measurement SCPI command. This user data can be provided in conjunction with a file path in the form of string key-value pairs. See example below.

Example: "/filepath.s2p","key=String Key 1,value=String Value 1","key=String Key 2,value=String Value 2"

You can also send the SCPI command with the file path specified as an empty string (see example below). In this case, the file name is automatically generated for the .s2p file with the provided user data.

Example: "","key=String Key 1,value=String Value 1","key=String Key 2,value=String Value 2"

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > Run Measurement

SCPI Command

[:SOURce][:RF<channel>]:CORRection: BLOCk2|3|4:FIXTure:CHARacterize:RUN <file_name>[,<userdata>]

SCPI Example

RF1:CORR:BLOC2:FIXT:CHAR:RUN

RF1:CORR:BLOC2:FIXT:CHAR:RUN "file.s2p"

RF1:CORR:BLOC2:FIXT:CHAR:RUN "file.s2p","key=FIXTURE serial,value=ABC123"

Couplings

When successful, sets Fixture Characterization Correction File to the resulting .s2p file and sets the correction block Enable to ON.

Notes

For instruments with Option V08:

  • Attempt to run while the calculated number of measurement points becomes 0 raises -200, “Execution error; Increase measurement points or a range of frequency"

For instruments without Option V08:

  • Attempting to run the measurement raises the error 703, "Feature not supported; Fixture Characterization unavailable on this instrument."

State Saved

No

Abort

Aborts Fixture Characterization measurement.

GUI Location

RF Output > Corrections/De-embedding > Block B, C, or D > Block Properties > Characterize > Run Measurement > Abort

SCPI Command

[:SOURce][:RF<channel>]:CORRection:BLOCk2|3|4:FIXTure:CHARacterize:ABORt

SCPI Example

RF1:CORR:BLOC2:FIXT:CHAR:ABOR

State Saved

No

Absolute Power Table Preset

Remote command only.

Initializes the Absolute Power table to a single point at the maximum frequency of the instrument with 0 dB correction.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:PRESet

SCPI Example

CORR:FLAT:PRES

State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:PRESet

Backwards Compatibility Notes

For N51xxB:

Expand [:SOURce]:CORRection:FLATness:PRESet to [:SOURce][:RF<channel>]:CORRection:FLATness:PRESet

Absolute Power Table Pair

Remote command only.

Inserts or updates a frequency/amplitude pair in the Absolute Power table.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:PAIR <freq>,<amplitude>

SCPI Example

CORR:FLAT:PAIR 1E9,-1.5

Notes The table is kept sorted by ascending frequency. The max pairs in the table are 3201.
State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:PAIR

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:PAIR to [:SOURce][:RF<channel>]:CORRection:FLATness:PAIR

Absolute Power Table Points

Remote command only.

Returns the number of frequency/amplitude pairs currently in the Absolute Power table.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:POINts?

SCPI Example

CORR:FLAT:POIN?

State Saved No
Min 0
Max 3201
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:POINts?

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:POINts? to [:SOURce][:RF<channel>]:CORRection:FLATness:POINts?

Absolute Power Table Frequency

Remote command only.

Query only command. Returns the frequency (in Hz) of the specified point in the Absolute Power table . <point> is a 1-based integer index.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:FREQuency? <point>

SCPI Example

CORR:FLAT:FREQ? 1

Notes If <point> is less than 1 or greater than the number of points in the table, raises error -224,"Illegal parameter value;Point index out of range."
State Saved No
Min 1
Max 3201
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:FREQuency?

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:FREQuency? to [:SOURce][:RF<channel>]:CORRection:FLATness:FREQuency?

Absolute Power Table Store

Remote command only.

Saves the current in-memory Absolute Power table to a file in the Corrections directory.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:STORe <"file">

SCPI Example

CORR:FLAT:STOR "myfile.csv"

CORR:FLAT:STOR "myfile.uflat"

CORR:FLAT:STOR "myfile.userflat"

CORR:FLAT:STOR "myfile"

Notes
  • The file format is determined by the file extension: .csv for CSV format, .uflat or .userflat for compatibility.

  • When no extension is provided and SCPI Backwards Compatibility Mode is set to N51xxB, .userflat is automatically appended to the filename. In all other modes, the file is saved in CSV format without an extension.

State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:STORe

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:STORe to [:SOURce][:RF<channel>]:CORRection:FLATness:STORe

Absolute Power Table Initialize Frequency Step

Remote command only.

Initializes the Absolute Power table with linearly spaced frequencies from Start Frequency to Stop Frequency using the configured Number of Steps. All amplitudes are set to 0 dB.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:FLATness:INITialize:FSTep

SCPI Example

:CORRection:FLATness:INITialize:FSTep

State Saved No
Backwards Compatibility SCPI

N51xxB

[:SOURce]:CORRection:FLATness:INITialize:FSTep

Backwards Compatibility Notes For N51xxB:
Expand [:SOURce]:CORRection:FLATness:INITialize:FSTep to [:SOURce][:RF<channel>]:CORRection:FLATness:INITialize:FSTep

DUT Reflection Coefficient

Overview

For the N5185A/N5186A with Option V08, this linear correction compensates for the instrument/DUT mismatch. This correction can be loaded via a specified .s1p file or can be measured to generate a .s1p file.

Any time the DUT's match changes so as to affect the measurement performance, it is recommended to remeasure and apply the DUT Reflection Coefficient correction.

To apply DUT Reflection Coefficient correction

  1. Select the DUT block displayed in the Corrections/De-embedding setup screen.

  2. From the DUT Reflection Coefficient section,

    • either click File > to specify a predefined .s1p file to be used for correction.

    • or click the Add from Measurement button to configure and run the DUT Reflection Coefficient measurement to generate a .s1p file for correction.

  3. Click the Enable checkbox to apply the correction stored in the .s1p file.

File

The specified .s1p file is applied when DUT Reflection Coefficient > Enable setting is ON.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:FILE <file_name>

[:SOURce][:RF<channel>]:CORRection:RCOefficient:FILE?

SCPI Example

RF1:CORR:RCO:FILE "corr.s1p"

RF1:CORR:RCO:FILE?

Preset

None

State Saved

Yes

Enable

Applies the DUT Reflection Coefficient Correction stored in the provided .s1p correction file.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:ENABle ON|OFF|1|0

[:SOURce][:RF<channel>]:CORRection:RCOefficient:ENABle?

SCPI Example

RF1:CORR:RCO:ENAB ON

RF1:CORR:RCO:ENAB?

Notes

For instruments without Option V08:

  • Attempting to set termination raises the error 703, "Feature not supported; Enable DUT Reflection Coefficient Correction."

For instruments with Option V08:

  • Attempting to turn ON without DUT Reflection Coefficient Correction File raises the error, -221, "Settings Conflict;DUT Reflection Coefficient Correction cannot be applied without a correction file."

Preset

None

State Saved

Yes

Range

OFF|ON

Center Frequency Corrections Only

Only applies the absolute power, phase and time corrections to the. s1p data.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:CFConly2[:STATe] ON|OFF|0|1

[:SOURce][:RF<channel>]:CORRection:CFConly2[:STATe]?

SCPI Example

CORR:CFC2 ON

CORR:CFC2?

Preset

0

State Saved

Yes

Backwards Compatibility SCPI

[:SOURce][:RF<channel>]:CORRection:APConly[:STATe]

Backwards Compatibility Notes

Alias [:SOURce][:RF<channel>]:CORRection:APConly[:STATe] to

[:SOURce][:RF<channel>]:CORRection:CFConly2[:STATe]

See Also - Block > Center Frequency Corrections Only

Delta

Query only. Reports the change in amplitude and phase flatness when DUT Reflection Coefficient > Enable setting is ON for the specified channel. For CW signals, this is a single value. For other signal types, this is an array of values versus frequency.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:DATA?

SCPI Example

RF1:CORR:RCO:DATA?

Notes

For instruments with Option V08:

  • Attempting to query data without DUT Reflection Coefficient Correction File raises error -221, "Settings Conflict;DUT Reflection Coefficient Correction Data cannot be queried without a correction file."

State Saved

No

Add from Measurement

You can use the Add from Measurement button to access the Measure DUT Reflection Coefficient screen. Using this screen, you can configure and run the DUT Reflection Coefficient measurement. The linear correction data generated from this measurement is saved to a .s1p file. This file is then used as the DUT Reflection Coefficient correction file.

Run Measurement

Runs the DUT Reflection Coefficient measurement.

Upon successful completion of this measurement:

Note that the measurement can be aborted by the Abort command.

Additionally, user data can be included in the resulting file’s header when specified via SCPI. This user data must be provided in conjunction with a file path in the form of string key-value pairs, see example 1. If an automatically generated filename is desired with user data provided, the command should be sent with the file path specified as an empty string, see example 2.

Example 1: "/filepath.s1p","key=String Key 1,value=String Value 1","key=String Key 2,value=String Value 2"

Example 2: "","key=String Key 1,value=String Value 1","key=String Key 2,value=String Value 2"

Reflection Coefficient can be measured on all single, dual, and quad channel configurations.

For information on Correction / De-embedding, see Corrections/De-embedding.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:RUN <"file path">[,<userdata>]

SCPI Example

RF1:CORR:RCO:RUN

RF1:CORR:RCO:RUN "file.s1p"

RF1:CORR:RCO:RUN "file.s1p","key=DUT serial,value=ABC123"

Couplings

When successful, sets DUT Reflection Coefficient Correction File to the resulting .s1p file and sets Apply DUT Reflection Coefficient Correction to ON.

Notes

For instruments with Option V08:

Attempting to run will raise the following errors/warnings depending on the conditions.

  • S11 measurement accuracy may be compromised when Corrections/Deembedding fixture's S-parameter includes S21 < -10 dB

  • S11 measurement accuracy may be compromised when Corrections/Deembedding fixture's S-parameter includes |S21 - S12| > 0.2 dB

State Saved

No

Abort

Aborts DUT Reflection Coefficient measurement.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:ABORt

SCPI Example

RF1:CORR:RCO:ABOR

State Saved

No

Measurement Start Frequency

Sets the start frequency for the DUT Reflection Coefficient Measurement correction point array.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:STARt <freq>

[:SOURce][:RF<channel>]:CORRection:RCOefficient:STARt?

SCPI Example

RF1:CORR:RCO:STAR 3GHz

RF1:CORR:RCO:STAR?

Couplings

Coupled to Stop Frequency.
If Start Frequency goes above Stop Frequency, Stop Frequency is automatically adjusted to Start Frequency.

Preset

1 GHz

State Saved

Yes

Min

9 kHz

Max

With Option 503 = 3 GHz

With Option 506 = 6 GHz

With Option 508 = 8.5 GHz

Resolution

0.00001 Hz

Measurement Stop Frequency

Sets the stop frequency for the DUT Reflection Coefficient Measurement correction point array.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:STOP <freq>

[:SOURce][:RF<channel>]:CORRection:RCOefficient:STOP?

SCPI Example

RF1:CORR:RCO:STOP 3GHz

RF1:CORR:RCO:STOP?

Couplings

Coupled to Start Frequency. If Stop Frequency goes below Start Frequency, Start Frequency is automatically adjusted to Stop Frequency.

Preset

2 GHz

State Saved

Yes

Min

9 kHz

Max

With Option 503 = 3 GHz

With Option 506 = 6 GHz

With Option 508 = 8.5 GHz

Resolution

0.00001 Hz

Measurement Number of Points

Defines the number of points in the DUT Reflection Coefficient Measurement correction step array. A frequency spacing of 10 MHz is optimal.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:POINts <integer>

[:SOURce][:RF<channel>]:CORRection:RCOefficient:POINts?

SCPI Example

RF1:CORR:RCO:POIN 1000

RF1:CORR:RCO:POIN?

Preset

850

State Saved

Yes

Min

2

Max

8500

Measurement IF Bandwidth

Defines the IF bandwidth for the DUT Reflection Coefficient Measurement. Reducing the IF receiver bandwidth reduces the effect of random noise on a measurement. Each tenfold reduction in IF bandwidth lowers the noise floor by 10 dB.

SCPI Command

[:SOURce][:RF<channel>]:CORRection:RCOefficient:BANDwidth <freq>

[:SOURce][:RF<channel>]:CORRection:RCOefficient:BANDwidth?

SCPI Example

RF1:CORR:RCO:BAND 100

RF1:CORR:RCO:BAND?

Preset

1 kHz

State Saved

Yes

Min

1 Hz

Max

100 MHz