Preset

The Preset button can be accessed from either the keypad or the multi-touch display, but each have unique behaviors.

Keypad access performs an immediate preset of the instrument

Multi-touch access opens a menu of options

Preset Menu

Preset

User Preset

Save User Preset

Preset Type

Types of Preset

Preset Menu

The preset functions provide known convenient starting points for individual mode settings. The green key on the multi-touch display allows you to choose between a preset of the whole instrument or a user preset (previously saved). Some preset functions are available through remote commands only. See also Types of Preset.

preset dropdown

Menu Choices:

Preset

User Preset

Save User Preset

Preset

preset

Returns the instrument to a known state. Preset restores all variables within the current configuration to a Preset state except for persistent variables. This includes all signals and all RF outputs.

There are some variables that are unaffected by a preset. These are called persistent variables. Each application will list its persistent variables; to reset these, perform Restore Defaults.

See Types of Preset for more information.

SCPI Command

:SYSTem:PRESet

SCPI Example

:SYST:PRES

Notes

  • This command is identical to *RST.

  • When floating licenses are used, licenses are returned to the server when a Preset is performed.

  • When SCPI backward compatibility mode is set to N51xxB, settings will preset to N51xxB default values if the default is within allowed limits. See SCPI Backwards Compatibility Mode.

Status Bits/OPC dependencies

Clears all pending OPC bits.

User Preset

Recalls a state previously saved using the Save User Preset function. Saving a user-preset state, allows you to define your own favorite state and recall it at the touch of a single button.

user preset

Because User Preset is actually a Recall State, rather than a predefined Preset, it works a little differently than Preset, in that it affects all of the variables that normally only reset on Restore Defaults, because these are included in State files.

A default User Preset file is provided, which simply matches the state after a Restore Defaults has been performed.

GUI Location

Preset > User Preset

SCPI Command

:SYSTem:PRESet:USER

SCPI Example

:SYST:PRES:USER:SAVE

! Save the User Preset

:SYST:PRES:USER

! Recall the User Preset

Notes

:SYST:PRES:USER:SAVE (Save User Preset) is used to save the current state as the user preset state.

If loading a User Preset file from a different instrument, some settings may be limited and coupled differently, since the capabilities of the mode may have changed from when the User Preset file was saved.

Status Bits/OPC dependencies

Clears all pending OPC bits.

Save User Preset

Saves the current state in a unique location for recall by User Preset.

Save User Preset can be executed from the Preset drop-down.

save user preset

All of the variables are saved, including those reset by Preset and those only reset by Restore Defaults, so when you subsequently select User Preset, the instrument returns to the exact same setup that existed when you pressed the Save User Preset control.

GUI Location

Preset > Save User Preset

SCPI Command

:SYSTem:PRESet:USER:SAVE

SCPI Example

:SYST:PRES:USER:SAVE

Notes

:SYST:PRES:SAVE creates the same file as if you requested a *SAV or a MMEM: STOR:STAT, except User Preset Save does not allow you to specify the filename or the location of the file.

Control Label

Save User Preset

Preset Type

Remote command only.

Defines whether the Preset action performs a factory preset or the user preset saved in memory.

SCPI Command

:SYSTem:PRESet:TYPE NORMal|USER

:SYSTem:PRESet:TYPE?

SCPI Example

SYST:PRES:TYPE NORM

SYST:PRES:TYPE USER

SYST:PRES:TYPE?

Dependencies

  • When set to USER, all three preset paths execute the user preset state saved in memory instead of the factory preset:

    • SCPI command :SYSTem:PRESet.

    • Physical front-panel Preset key

  • This command does not affect User Preset, which always recalls the user preset regardless of this setting.

  • Sending USER when no user preset has been saved raises error -257,"File name error;User preset file could not be found: a user preset state must be saved before the preset type can be set to User."

  • To save a user preset first, use Save User Preset.

Preset This setting is unaffected by Preset. It is reset to NORMal on Restore System Settings to Default Values.
Range NORMal|USER
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.
Backwards Compatibility SCPI

N51xxB

:SYSTem:PRESet:TYPE

Types of Preset

The table below shows all possible presets, their corresponding SCPI commands and front-panel access methods.

To get back to a fully predefined user state, you should execute a Factory Preset.

Type Of Preset

SCPI Command

Scope of Preset

Front Panel Access

Preset

:SYSTem:PRESet

*RST

Restores all variables to a Preset state except for Persistent variables.  Includes all signals and all RF Outputs

Preset (green key) and Preset in the Preset drop-down menu on multi-touch display

User Preset

:SYSTem:PRESet:USER

Restores all variables to the saved User Preset state including Persistent variables.  System Settings are unaffected.  Includes all signals and all RF Outputs

User Preset in the Preset drop-down menu on multi-touch display

Restore System Settings to Default Values

:SYSTem:PRESet:PERSistent

Only the instrument’s persistent settings are returned to their factory default values.

System Menu > Settings > Power On/Preset > Restore System Defaults and Power On/Preset

Factory Preset

:SYSTem:PRESet:ALL

 

 

Restores all variables to a Preset state including Persistent variables and System Settings. 

System Menu > Settings > Power On/Preset > Restore System Defaults and Power On/Preset

Power On/Standby (Instrument Shutdown)