Status

The Status icon opens a screen showing important instrument conditions. You can interact with any of its information fields to open associated user-interface screens. A red exclamation mark in the status icon indicates an instrument condition requiring attention.

RF Out (All)

For multi-channel capability only.

Turns the RF outputs on or off for all the channels in the instrument. This is a master control that gates the individual states. If this control is off, no RF power is emitted from any of the channels; however, the individual channels retain the state of their setting. If this control is on, the RF outputs are on if their individual state is on. To enable or disable individual channels see RF Out.

For more information, see RF Out (All).

1. Reference Indicator

The Reference indicator provides visual indication of the source of the reference (Internal or External) and its current state. Refer to Reference to know more.

In the Reference Indicator, the source of the Reference can be shown as one of the following:

Source Indicator Description
INT Internal
EXT External
INT(A)

Internal Auto

Indicates that the Reference Source is set to Auto and the current Reference Source being automatically applied to the instrument is Internal.

EXT(A)

External Auto

Indicates that the Reference Source is set to Auto and the current Reference Source being automatically applied to the instrument is External.

In the Reference Indicator, the state of the Reference can be shown as one of the following:

2. Synchronization Status

This field reports the current synchronization status. Refer to Triggers and Sync > Synchronization.

3. GPIB/Remote Annunciators

The GPIB/Remote annunciators are shown as the letters KRLT and S. Each letter is bright if the state is true and is dim if the state is false, as follows:

Refer to I/O Configuration.

4. Clock

This field displays the instrument's clock, including the date and time. Refer to Instrument Information.