E-DPCCH/E-DPDCH TTI Pattern Selection for Advanced UL
Use this dialog box to set the TTI pattern with either MAIN or ALT (alternate) E-TFCI table selections for each of the 15,330 slots. The flexibility of the software allows the start of a TTI period at any point in the available slots.
The Number of Frames cell in the advanced carrier view determines the length of the waveform. If the configured pattern length exceeds the waveform length, the software ignores the excess pattern slots.
Descriptions
This list enables you to quickly access the different areas of the dialog box.
Main All
The channel only uses the table identified in the cell and the cell.
User
This selection enables the dialog box editor and allows the user to customize TTI patterns for up to 15,330 slots (1022 frames).
Import
This button loads a user-defined pattern from a selected location. When you select this button, the dialog box appears for navigating to and selecting the desired file. An imported file automatically updates the area. The software accepts the following file types:
-
ASCII text
-
comma separated values (csv)
To create a file, enter five parameters per slot: frame number, slot number, power level, state (0 or 1), and the text MAIN or ALT:
For example, to set slots 0 and 3 for frame 0, and slots 2 and 5 for frame 2, use the following format:
0,0,-10 dBm,1,ALT,0,3,-5 dB,1,ALT,2,2,1 dB,1,MAIN,2,5,5 dB,1,ALT
The power unit, and the space between the power value and dB is not required. If desired, place each slot setting on a separate line:
0,0,-10,1,ALT,
0,3,-5,1,ALT,
2,2,1,1,MAIN,
2,5,5,1,ALT
The maximum file size should not exceed the data required to set the maximum number of slots: 15,330, and the number of configured slots cannot exceed the waveform length.
Export
This button saves the current pattern, showing in the area, to a file. When you select this button, a dialog box appears for navigating to the location where you can save the file. The software saves the user data as one of the following user-selectable file types:
-
ASCII text
-
comma separated values (csv)
Clear
This button clears the TTI Pattern table and sets as the selection with the column left unchecked and the power set to 0.00 dB for all slots..
TTI Pattern
Use this table to manually set the state (on = checked) and power level, and select either or for each slot.
TTI Pattern Descriptions |
|
Frame
Displays the frame number (0–1021). The frame number increments after every 15 slots.
Slot
Displays the slot number (0–14) for each frame. The slot numbers repeat after every 15 slots. The TTI cell setting determines the number of slots per TTI period.
The software supports a maximum of 15,330 slots. The number of configured slots cannot exceed the waveform length.
State
Manually set the state to either on (checked) or off for a TTI period. A TTI period (3-slots over 2 ms or 15 slots over 10 ms) starts with the first active (on) slot and last for the remaining consecutive slots in the TTI period regardless of whether the remaining TTI slots are on or off. The TTI period uses the settings (, , and or ) of the first slot in the TTI and ignores the settings of the remaining slots that are part of the TTI period. If a slot is not part of a TTI, it is DTX.
Power
Range: -60 to 20 dB
Manually set the power level for each slot. The bursting pattern uses the RMS of the carrier power as the absolute burst amplitude. During the power search the signal source uses the highest amplitudes of the channels (slot power + channel power) to find the RMS value. When you download the waveform, the software initiates an instrument power search.
When the waveform resides in an instrument's non-volatile memory and is loaded into volatile memory, manually perform an instrument RMS power search. For more information on performing an instrument power search, refer to the instrument's User Guide. You may also perform the RMS power search. from the software interface.
MAIN
Sets the slot to use the following cell settings in the E-DPCCH and E-DPDCH views:
|
Settable |
Grayed Out—Information Only |
|
ALT
Sets the slot to use the following alternate cell settings in the E-DPCCH and E-DPDCH views:
|
Settable |
Grayed Out—Information Only (Located on only the E-DPDCH) |
Tool
Use this table to set up and apply a repeating TTI pattern set to either or . A TTI period (3-slots over 2 ms) starts with the first active (on) slot and last for three consecutive slots regardless of whether the remaining two slots are on or off. The TTI period uses the settings (, , and or ) of the first slot in the TTI and ignores the settings of the two remaining slots. If a slot is not part of a TTI, it is DTX.
Tool Descriptions |
|
Start
Range: 0 to 15329
Set the starting slot number offset. While the table slot numbers (0–14) repeat for each frame, the Start values continuously increments up to the maximum range value. For example, to start the pattern on frame 2, slot 10, set this cell's value to 40. To set slot 5 in frame 8, set the Start value to 125.
This setting accepts values that are smaller or larger than the range values. When the software recognizes a value that is outside of the range, it ignores the value.
Step
Range: 0 to 15329
This cell sets the pattern of transmitted slots by setting the interval of active slots. For example with a value of two, the software sets a repeating pattern for every other slot starting with the slot identified in the cell and ending with the number of repetitions identified in the cell. The number of configured slots cannot exceed the waveform length.
|
0 |
The pattern consists of only the slot identified with the starting value and ignores the repeat value |
|
1...15329 |
The value determines whether the pattern transmits all slots from the Start value to the Repeat value or includes an integer number of DTX slots between each transmitted slot:
|
This setting accepts values that are smaller or larger than the range values. When the software recognizes a value that is outside of the range, it ignores the value.
Repeat
Range: 0 to 15330
Sets the end slot number for the pattern. The number of configured slots cannot exceed the waveform length.
|
0 |
No slots are set. |
|
1...15330 |
The value determines the number of configured slots.
|
If this value is larger than the number of remaining slots from the Start value to the last slot, then all remaining slots are included in the pattern.
Power
Range: -60 to 20 dB
Sets the power level for the slots in the pattern. If needed and after applying the pattern, manually adjust the power level on individual checked slots. The bursting pattern uses the RMS of the carrier power as the absolute burst amplitude. During the power search the signal source uses the highest amplitudes of the channels (slot power + channel power) to find the RMS value. When you download the waveform, the software initiates an instrument power search.
When the waveform resides in an instruments non-volatile memory and is loaded into volatile memory, manually perform an instrument RMS power search. For more information on performing an instrument power search, refer to the instrument's User Guide. You may also perform the RMS power search. from the software interface.
Fill Pattern
Choice: MAIN or ALT
Sets the pattern to use either MAIN or ALT. After clicking in the cell, a down arrow button appears; click the button to display and make the selection.
Apply Pattern (Button)
Applies the repetition pattern to the TTI Pattern table.