The carrier configuration summary
table
is the same in this view as it appears in the view, along with the functions of each of the buttons located
directly above the summary table. This means that you can select, add, and delete carriers from thecarrier view.
Select a
carrier
in the carrier configuration summary table or select a carrier from the
tree view.
Select > .
Having the status window open provides greater visibility to errors. Error messages appear in two places: in the status bar at the bottom of the UI, and in the status window. In the status window, they appear with a large red dot, which helps to alert you an error. The status window also lists all uncorrected errors, whereas the status bar only shows the most recent uncorrected error.
Configure the carrier parameters for either downlink or uplink as dictated by the carrier selection.
When you select another predefined channel setup, it replaces the channel configuration showing in the configuration summary table for the current carrier. This causes the loss of any previously configured channel settings, unless those particular configurations have been saved.
Select a carrier from either the summary table or tree view.
Select the cell.
Click the drop-down arrow that appears at the far right of the row.
From the dialog box that appears, select a predefined configuration for the current carrier.