Click
or
from the main tool bar
to generate an I/Q waveform and plot four different waveform graphs (Power,
I+Q, I/Q, and Spectrum) in accordance with the current
channel configuration. Any changes to the channel configuration do not
appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform
generation progress.
plot shows the cumulative power of the carrier configuration.
Click this button to select from the list of different waveform plots.
Selections include Power (shown above),
I+Q,
I|Q,
and
Spectrum.
Click the arrow to access a drop-down menu where you can make a direct
selection. Clicking the button selects the next plot type in the list
without displaying the menu.
The Waveform and CCDF graphs are minimized in
the Waveform Setup node's initial view. To view the graphs, click and
drag the
border
above the CCDF and Waveform graphs.