High-speed Uplink Packet Access (HSUPA) offers greater efficiencies with the following:
transport channel Enhanced Dedicated Channel (E-DCH) and
physical channels:
See also HARQ Process States.
|
1. General Settings |
|---|
This section defines the Settings Current and Apply Needed buttons. Only one button is available at any time. These buttons are available in all of the W-CDMA/HSPA+ Uplink's tree nodes.
|
|
This button indicates that the current real-time settings have been applied to the instrument. No action is required. |
|
|
This button indicates that the instrument settings are not current and need to be updated to be applied to the instrument. Click this button to update the instrument's settings. [:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:APPLy [:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:APPLy? |
Choice: Off | On
Default: On
Enables or disables the HSUPA state. This field controls the state of E-DPDCH and E-DPCCH.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa[:STATe] ON|OFF|1|0
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa[:STATe]?
Choice: 2 | 10 (ms)
Default: 10 ms
Sets the transmission time interval (TTI) of HSUPA in ms.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TTI 2|10
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TTI?
Choice: None | IR (Incremental Redundancy) | CC (Chase Combining)
Default: None
Sets the HARQ mode. This field controls signaling pattern of HARQ.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ[:MODE] NONE|IREDundancy|CCOMbining
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ[:MODE]?
Range: 0 to 3
Default: 0
Set Retransmission Sequence Number (RSN). This field is enabled when HARQ mode is set to None.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:RSN 0|1|2|3
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:RSN?
Range: 0 to 3
Default: 0
Sets the Redundancy Version (RV) Index. This field is enabled when HARQ Mode is None.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:RVINdex 0|1|2|3
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:RVINdex?
Range: 0 to 15
Default: 15
Sets the maximum number of HARQ retransmission. This field is disabled when HARQ mode is None.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:MNRTrans <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:MNRTrans?
Choice: ACK All | Custom Pattern| User File | External
Default: ACK All
Edit the HARQ ACK/NACK Pattern by clicking on the cell. Then click on the dialog box icon
to launch the
HARQ ACK/NACK Pattern dialog box.
When loading a user file through the software's Data dialog box, the MXG/EXG requires an ASCII text file consisting of 1s and 0s. When using SCPI commands, all instruments require a binary data file.
|
ACK All |
This choice configures 1,280 subframes (if TTI=2ms) or 1,280 frames (if TTI=10ms) for a simulated ACK only response. |
|
Custom Pattern |
Sets the HARQ ACK/NACK data pattern to Custom Pattern. The value of this command is a string which is represented ‘0’ or ‘1’. The maximum data length is 18,000 patterns. |
|
User File |
This variable represents an ACK pattern file stored in instrument memory. |
|
External |
Sets the HARQ ACK/NACK data pattern to External. This choice specifies an external HARQ ACK/NACK pattern. |
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:APATtern ACK_ALL|NACK_ALL|EXTernal|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:APATtern?
If you select PATTern, use the following commands to create the pattern:
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:APATtern:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:APATtern:PATTern?
Range: 0 to 115200 (TTI = 10ms), 0 to 53760 (TTI = 2ms),
Default: 7680, Resolution: 256
Sets the delay of the external trigger for the HARQ ACK/NACK Pattern. Refer to External Input-Based HARQ Scheduling (TTI = 2 ms) and to External Input-Based HARQ Scheduling (TTI = 10 ms).
Couplings:
HSUPA State = On,
HARQ Mode = IR or CC, and
HARQ ACK/NACK Pattern = External.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:APATtern[:EXTernal]:DELay <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HARQ:APATtern[:EXTernal]:DELay?
Choice: Main All | External| Custom Pattern | User File
Default: Main All
Edit the TFC E-TFCI Pattern by clicking on the cell. Then click on the dialog box icon
to launch the
TFC E-TFCI Pattern dialog box.
When loading a user file through the software's Data dialog box, the MXG/EXG requires an ASCII text file consisting of 1s and 0s. When using SCPI commands, all instruments require a binary data file.
|
Main All |
This choice configures all subframes for a simulated MAIN only response. |
|
External |
This choice selects an external signal to control the data pattern. |
|
Custom Pattern |
Sets the TFC E-TFCI data pattern to Custom Pattern. The value of this command is a string which is represented ‘0’ or ‘1’. The maximum data length is 18,000 patterns. |
|
User File |
This variable represents a MAIN/ALT pattern file. Create this file using the TFC pattern Data Type Entry window and download the file to the instrument. Create a bit file with the following bit patterns:
|
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC:EPATtern MAIN|EXTernal|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC:EPATtern?
If you select <"filename"> or PATTern, use the following commands to create the pattern:
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC:EPATtern:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC:EPATtern:PATTern?
Range: 0 to 115200 (TTI = 10ms), 0 to 53760 (TTI = 2ms)
Default: 7680, Resolution: 256
Sets the delay of the external trigger for the TFC E-TFCI Pattern.
[:SOURce]:RADio:WCDMa:TGPP:ULINk:HSUPa:TFC:EPATtern[:EXTernal]:DELay <val>
[:SOURce]:RADio:WCDMa:TGPP:ULINk:HSUPa:TFC:EPATtern[:EXTernal]:DELay?
Choice: 0 | 1
Default: 1
Sets the table number of E-DCH Transport Block Size Table for the main setting.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:ETABle 0|1
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:ETABle?
Choice: 0 | 1
Default: 1
Sets the table number of E-DCH Transport Block Size Table for the alternate setting. This field is disabled when TFC E-TFCI Pattern is "Main All".
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:ETABle 0|1
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]ETABle?
Range: 0 to 127 (TTI = 2ms, E-TFCI Table Selection = 0)
Range: 0 to 125 (TTI = 2ms, E-TFCI Table Selection = 1)
Range: 0 to 127 (TTI = 10ms, E-TFCI Table Selection = 0
Range: 0 to 120 (TTI = 10ms, E-TFCI Table Selection = 1)
Default: 41
Sets E-TFCI Index for the main setting.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:ETFCi <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:ETFCi?
Range: 0 to 127 (TTI = 2ms, E-TFCI Table Selection = 0)
Range: 0 to 125 (TTI = 2ms, E-TFCI Table Selection = 1)
Range: 0 to 127 (TTI = 10ms, E-TFCI Table Selection = 0
Range: 0 to 120 (TTI = 10ms, E-TFCI Table Selection = 1)
Default: 41
Sets E-TFCI Index for the alternate setting. This field is disabled when the TFC E-TFCI Pattern is "Main All".
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:ETFCI <value>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]ETFCI?
Choice: Happy | Not Happy | Custom Pattern | User File
Default: Happy
Edit the Happy Bit by clicking on the cell. Then click on the dialog box icon
to launch the
Happy Bit dialog box.
When loading a user file through the software's Data dialog box, the MXG/EXG requires an ASCII text file consisting of 1s and 0s. When using SCPI commands, all instruments require a binary data file.
|
Happy |
This choice sets the happy bit to happy. |
|
Not Happy |
This choice sets the happy bit to not happy. |
|
Custom Pattern |
This choice sets the custom pattern for entering the number of Happy or Not Happy bit patterns. |
|
User File |
This variable represents a happy bit pattern file. Create this file by using the Happy Bit Pattern Data Type Entry window and download the file to the instrument. Create a bit file with the following bit patterns:
|
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HBIT HAPPy|NHAPpy|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HBIT?
If you select PATTern, use the following commands to create the pattern:
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HBIT:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:HBIT:PATTern?
Choice: Process | Custom Pattern | User File
Default: Process
Edit the HSUPA DTX Control Mode by clicking on the cell. Then click on the dialog box icon
to launch the
HSUPA DTX Control Mode dialog box.
When loading a user file through the software's Data dialog box, the MXG/EXG requires an ASCII text file consisting of 1s and 0s. When using SCPI commands, all instruments require a binary data file.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:DTXMode PROCess|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:DTXMode?
If you select <"filename"> or PATTern, use the following commands to create the pattern::
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:DTXMode:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:DTXMode:PATTern?
Range: 18 to 20000
Indicate the block size of HSUPA transport channel (E-DCH). This item is called "Information Bit Payload (N-INF)" in TS 25.141.