Channels, controls the states and power levels for the uplink channels. Also, displays the channel coding, spreading factor (SF), and data-type information.
Refer to RMC FRC Wizard and to Channels DPCCH/DPDCH).
| Channel | Enables or disables the channel state. The E-DPCCH and E-DPDCH states are shown by the combination result of the HSUPA and E-DPCCH/E-DPDCH states. When the E-DPCCH or E-DPDCH state is set to On, the state of HSUPA is also set to On. |
| State | Enables or disables the channel state. The E-DPCCH and E-DPDCH states are shown by the combination result of the HSUPA and E-DPCCH/E-DPDCH states. When the E-DPCCH or E-DPDCH state is set to On, the state of HSUPA is also set to On. |
| Power (dB) | Sets the power level in dB. The Alt field is disabled when the TFC E-TFCI Pattern is set to "Main All". |
| Code | Indicates the channel code. |
| Spreading Factor (SF) | Indicates the spreading factor. |
| Data | Indicates the data pattern. |