These setting control the PRACH real-time Channel Settings.
Refer to Code Domain Graphics and to RMC/FRC Wizard (DPCCH/DPDCH).
|
1. General |
|---|
This section defines the W-CDMA/HSPA+ DPCCH/DPDCH's buttons. With the exception of the RMC/FRC Wizard button, the Restore Default Settings button is available in all of the W-CDMA/HSPA+ Uplink (DPCCH/DPDCH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
|
Opens the RMC/FRC Wizard window for the channel. |
Range: 0 to 16777215
Default: 0
Sets the scrambling code number.