The Dedicated Physical Data Channel (DPDCH) transmits the higher layer information (e.g. user data, ...).
|
1. DPDCH |
2. DPDCH Data |
3. Transport Channel BER |
|---|---|---|
|
|
||
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
This section defines the W-CDMA/HSPA+ DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the W-CDMA/HSPA+ Uplink (DPCCH/DPDCH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
Choice: Off | On
Default: On
Enables or disables the DPDCH state.
Range: -40 to 0 dB
Default: 0 dB
Enter the DPDCH power level in dB.
Range: 0 to 255 (Slot format = 0),
0 to 127 (Slot format = 1),
0 to 63 (Slot format = 2),
0 to 31 (Slot format = 3),
0 to 15 (Slot format = 4),
0 to 7 (Slot format = 5),
0 to 3 (Slot format = 6)
Default: 16
Sets the channel code of DPDCH. This field is enabled when HS-DPCCH and HSUPA (E-DPCCH/E-DPDCH) channel states are set to Off. Indicates the calculated channel code of DPDCH when HS-DPCCH and/or HSUPA channel states are set to On.
Range: 0 to 6
Default: 2
Sets the slot format of DPDCH. This value is coupled to Symbol Rate.
Selection: 15 ksps | 30 ksps | 60 ksps | 120 ksps | 240 ksps | 480 ksps | 960 ksps
Default: 60 ksps
Sets the Symbol Rate (symbol per second: sps) for DPDCH. This value is coupled to Slot Format.
Indicates the Spreading Factor for DPDCH.
Choice: 0 | 1
Default: 0
Sets the maximum number of DPDCH (Nmax-dpdch) to control channel assignment.
This field is available when the DPDCH State is Off. When DPDCH State is On, this field is always 1.
Choice: PN9 | PN15 | FIX4 | DCH|Custom Pattern| User Data
Default: DCH
Sets the data pattern for the dedicated physical data channel (DPDCH).
Where User File is selected, the data file must be in binary format and specify the bit length.
Range: 1 to 6
Default: 2
Sets the number of DCH for DPDCH coding source.
Range: 0 to 1
Default: 0
Indicates the value of the DPDCH Transport channel BER. This value is calculated by the DPDCH Transport channel BER cycle length and the error insertion length.
Range: 0 to 65535
Default: 0
Sets the cycle length of the DPDCh Transport channel BER. This value is set to 0, the insertion of the transport channel BER is disabled.
Range: 0 to 4095
Default: 0
Sets the error insertion length of the DPDCH Transport channel BER.