In the uplink, the Enhanced Dedicated Physical Data Channel (E-DPDCH) is the physical channel used by the Enhanced Dedicate Control Channel (E-DCCH) to transmit user data.
|
1. E-DPDCH |
2. E-DCH |
|---|---|
|
|
|
|
Miscellaneous Information (E-DCH) |
|
|
|
|
|
Miscellaneous Information (E-DPDCH) |
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
This section defines the W-CDMA/HSPA+ DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the W-CDMA/HSPA+ Uplink (DPCCH/DPDCH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
Choice: Off | On
Default: On
Enables or disables the E-DPDCH state.The HSUPA State is needed to be also "On" to enable the E-DPDCH data generation.
Range: -40 to 0 dB
Default: 0 dB
Set the E-DPDCH power in dB. This power is assigned to each E-DPDCH when multiple E-DPDCHs are configured. The entered power is typically set to the channels as SF4. Where the E-DPDCHs are configured to SF2x2 + SF4x2, the channel power of SF2 is 3.01 dB higher than the entered power.
Range: -40 to 0
Default: 0
Set the power of the alternate E-DPDCH setting in dB. This field is disabled when TFC E-TFCI Pattern is MAIN ALL. This power is assigned to each e_DPDCH when multiple E-DPDCHs are configured. The entered power is set to the channels as SF4. Where the E-DPDCHs are configured to SF2x2 + SF4x2, the channel power of SF2 is 3.01 dB higher than the entered power.
Choice: SF256 (x1) | SF128 (x1) | SF64 (x1) | SF32 (x1) | SF16 (x1) | SF8 (x1) | SF4 (x1) | SF4 (x2) | SF2 (x2) | SF2 (x2) + SF4 (x2 )| AUTO
Default: SF4 (x1)
Select Spreading Factor (SF) and Number of E-DPDCHs configuration on the main setting.
HSUPA TFC E-TFCI Pattern should set to "Main All" when this value is set to "AUTO".
Choice: SF256 (x1) | SF128 (x1) | SF64 (x1) | SF32 (x1) | SF16 (x1) | SF8 (x1) | SF4 (x1) | SF4 (x2) | SF2 (x2) | SF2 (x2) + SF4 (x2)
Default: SF4 (x1)
Select Spreading Factor (SF) and Number of E-DPDCHs configuration on the alternate setting. This field is disabled when TFC E-TFCI Pattern is MAIN ALL.
Choice: SF256 (x1) | SF128 (x1) | SF64 (x1) | SF32 (x1) | SF16 (x1) | SF8 (x1) | SF4 (x1) | SF4 (x2) | SF2 (x2) | SF2 (x2) + SF4 (x2)
Default: SF2 (x2) + SF4 (x2)
Select Spreading Factor (SF) and the number of E-DPDCHs configuration. This field is enabled when SF and Number of E-DPDCHs is "AUTO".
Choice: QPSK (2 x BPSK) | 16QAM (2 x 4PAM)
Default: QPSK (2 x BPSK)
Set the E-DPDCH modulation capability
Range: 0.44 to 1.0
Default: 0.44
Set the PL non-max E-DPDCH setting. This field is enabled when SF and Number of E-DPDCHs is AUTO.
Choice: PN9 | FIX4 | Standard | Custom Data | User Data
Default: E-DCH
Sets the E-DPDCH data pattern. When E-DCH is selected, this applies the defined data in the E-DCH data and to the E-DCH coding.
Where User File is selected, the data file must be in binary format and specify the bit length.
Indicates the Binary Channel Bits per TTI (N-BIN). The alternate field is disabled when TFC E-TFCI Pattern is set to MAIN ALL.
Indicates the IQ branch assignment [I or Q] of E-DPDCH. When multiple E-DPDCHs are configured, multiple IQ assignment are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL.
Indicates the E-DPDCH Channel Code that is currently configured. When multiple E-DPDCHs are configured, multiple Channel Code assignments are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL.
Indicates the E-DPDCH Spreading Factor(s) that is currently configured. When multiple E-DPDCHs are configured, multiple Spreading Factor assignments are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL.
Indicates the E-DPDCH Bit Rate [kbps] that is currently configured. When multiple E-DPDCHs are configured, multiple bit rate assignments are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL.
Choice: PN9 | FIX4 | Custom Pattern | User Data
Default: PN9
Selects the data of the E-DCH.
Where User File is selected, the data file must be in binary format and specify the bit length.
Choice: PN9 | FIX4 | User Data
Default: PN9
Sets the data of the alternate E-DCH. This field is disabled when the TFC E-TFCI Pattern is set to Main All.
Indicates the CRC Length of E-DCH
Indicates the Coding Type of E-DCH.
Indicates the Coding Rate of E-DCH.
Indicate the Puncture Rate [%]. The puncture rate should be greater than 33 %.
Puncture Rate [%] = Ne,data,j / Ne,j * 100. [defined in 3GPP STD TS 25.212 4.8.4.1]