SCPI Commands without GUI Functions

The software provides a standard list of commands created for this software. The list also provides links to the command descriptions.

These commands have no corresponding UI Parameters, but set the real-time baseband for instruments loaded with Signal Studio (N7601C-WFP).

Use this topic to find SCPI commands that do not have corresponding UI parameters supported by either of the N5172B EXG and the N5182B MXG vector signal generators; or the N5106A PXB Baseband Generator and Channel Emulator.

E4438C Compatible Commands

For more detailed information on real-time E4438C compatible commands, for your instrument, refer to the E4438C Compatible Commands with the N5172B/82B topic.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:NOISe:CN <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:NOISe:CN?

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:NOISe[:STATe] ON|OFF|1|0

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:NOISe[:STATe]?

UI Parameter: n/a

Description

This command sets the carrier to noise ratio for the reverse link.

The variable <val> is expressed in units of decibels (dB).

*RST: +0.00000000E+000

Range: −30 to 30

Key Entry:  C/N

The carrier to noise ratio is the ratio of the carrier power to in-channel noise

power, expressed in decibels (dB).

A change to the carrier to noise ratio will only align the EbNo/EcNo field values

in the active operating mode.