For information about using the software to change instrument settings:
see Instrument for ARB capability with most signal generators
see Instrument (E6640A) for ARB capability with the E6640A EXM
see Instrument (MXG/EXG Real-Time Software) for real-time capability
Click Hardware in the tree view to display read-only information about the hardware.
When using a simulated instrument connection,
the
property page
shows <Simulated Hardware> in the
cell and <Simulated (instrument type)> appears in the
cell. N/A
appears in most of the other cells.
Click this button to run a test of the I/O interface connection between the instrument and the PC. performs the same tests as the button.
The Self-Tests
window
appears and displays the results of the tests. Closing the test dialog
window also closes the hardware node and opens the waveform setup node.
If an error occurs, a
red X
appears next to the failed test and an error message is displayed in the
status area.
Click this button to run a test of the I/O interface connection between the instrument and the PC. performs the same tests as the button.
The Test I/O Connections
window
appears and displays the results of the tests. Closing the test dialog
window also closes the hardware node and opens the waveform setup node.
If an error occurs, a
red X
appears next to the failed I/O connection and an error message is displayed
in the status area.
View the name assigned to the system.
View the hardware configuration type.
View connection details (LAN or GPIB).
View the instrument model number.
View the instrument serial number.
View the instrument firmware revision number.
View the options of the connected instrument. These cells are not displayed when using simulated hardware.