The following table shows the relationship between frequency band, ARFCN, and frequency.
For more information go to http://wireless.keysight.com/rfcomms/refdocs/gsmgprs/gen_bse_cell_band.php
|
Frequency Band |
Uplink/Downlink Separation |
Downlink Frequency Range (Transmit Device = Base) |
ARFCN |
|
|---|---|---|---|---|
|
GSM 450 |
10 MHz |
450.4 to 457.6 MHz |
460.4 to 467.6 MHz |
259 to 293 |
|
GSM 480 |
10 MHz |
478.8 to 486 MHz |
488.8 to 496 MHz |
306 to 340 |
|
GSM 750 |
30 MHz |
747 to 762 MHz |
777 to 792 MHz |
438 to 511 |
|
GSM 850 |
45 MHz |
824 to 849 MHz |
869 to 894 MHz |
128 to 251 |
|
P-GSM 900 |
45 MHz |
890 to 915 MHz |
935 to 960 MHz |
1 to124 |
|
E-GSM 900 |
45 MHz |
880 to 915 MHz |
925 to 960 MHz |
0 to124 and 975 to 1023 |
|
R-GSM 900 |
45 MHz |
876 to 915 MHz |
921 to 960 MHz |
0 to124 and 955 to 1023 |
|
DCS 1800 |
45 MHz |
1710 to 1785 MHz |
1805 to 1880 MHz |
512 to 885 |
|
PCS 1900 |
45 MHz |
1850 to 1910 MHz |
1930 to 1990 MHz |
512 to 810 |
The examples below show how the software sets the frequency after you enter the Frequency Band, the ARFCN, and select Mobile or Base as the Transmit Device.
In the figure below, the frequency band is selected with as the Transmit Device. The corresponding frequency range from the table is 935 to 960 MHz. The entry of forARFCN causes the software to set the frequency at the upper limit of the frequency range for (959.8 MHz).
Click the Generate Waveform button
to update the frequency setting.
In the example below, the ARFCN is set to . The Frequency Band remains set at and Transmit Device remains set at . When the waveform is generated, the software sets the frequency to the lower limit of the frequency range for (935.2 MHz).