Choice: On | Off
Default: On
Double-click or use the drop-down menu to set the state of the timeslot or .
Range: –70 to 0 dB.
Default: 0 dB
Enter a value to set the timeslot power.
View the data type. The data type is set by the software. You cannot edit this cell.
Range: 0 to 32767
Default: 0
Enter a data offset value to use when generating the data stream.
View the modulation type.
GSMK for GSM continuous pattern
8PSK and 3pi/8 rotation for EDGE continuous pattern
You cannot edit this cell.