SCPI Command List
NOTES:
1. In the SCPI command syntax, the letter n equates to a numeric value.
2. The following SCPI command list may include duplicates of certain commands. This duplication offers you the convenience of accessing a command's related descriptions when it is valid for more than one instrument model or channel type, and therefore, appears in multiple help topics.
[:SOURce]:FSIMulator[1]:FADer[1]:DLENgth <val>
[:SOURce]:FSIMulator[1]:FADer[1]:DLENgth?
[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency <val>
[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency?
[:SOURce]:FSIMulator[1]:FADer[1]:MODE ON | OFF | THR
[:SOURce]:FSIMulator[1]:FADer[1]:MODE?
[:SOURce]:FSIMulator[1]:FADer[1]:SDEViation <val>
[:SOURce]:FSIMulator[1]:FADer[1]:SDEViation?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:EDELay <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:EDELay?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:ELOSs <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:ELOSs?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSIDistance <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSIDistance?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSMDistance <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSMDistance?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:MDFRequency <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:MDFRequency?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:TSPeed <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANDard:LTE:HSTrain:TSPeed?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel DEFault | <SISO_Channel_Model_Name>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DBSPacing <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DBSPacing?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DTIMe <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DTIMe?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSIDistance <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSIDistance?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSMDistance <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSMDistance?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:MDFRequency <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:MDFRequency?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:TSPeed <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANDard:WCDMa:HSTrain:TSPeed?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MAXDelay <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MAXDelay?
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MINDelay <val>
[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MINDelay?