Status Bar

The status bar at the bottom of the window updates in real-time to show the status of running operations, such as waveform generation and downloading. Software licensing information for the signal generator is also displayed here. 

The status bar is divided into the following three sections:

Run Status Section

This section shows the status of the software's setup.

The following are some of the possible run status messages:

Initializing...

The software is setting up system parameters when the program starts.

Ready

The program successfully initialized.

Opening the settings file...

The program is reading the parameters from the settings file.

Saving the settings file...

The program is saving the parameters to a settings file.

Connection Status Section

This section shows the connection status of the software to the signal generator.

The following are some of the possible run status messages:

Blank (no text)

Simulated hardware mode.

Connected

The instrument connection is checked and verified.

Not Connected

The software cannot connect to the signal generator.

Software Message Section

This section shows license status, waveform generation progress, and error information for your setup. To view messages for multiple errors, use the status window.