Go to description Go to description Go to topic Go to topic Go to topic Go to description Go to description Go to description Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to description Go to description Go to description Go to description Go to topic Go to topic Go to topic Go to description Go to description

2. PDU Header Setting

PDU header settings vary according to the selected Packet Type.

ADV_IND, ADV_NONCONN_IND, SCAN_RSP, ADV_SCAN_IND

ADV_DIRECT_IND, SCAN_REQ, CONNECT_REQ

LL_DATA, LL_CONNECTION_UPDATE_REQ, LL_CHANNEL_MAP_REQ, LL_TERMINATE_IND, LL_ENC_REQ, LL_ENC_RSP, LL_START_ENC_REQ, LL_START_ENC_RSP, LL_UNKNOWN_RSP, LL_FEATURE_REQ, LL_FEATURE_RSP, LL_PAUSE_ENC_REQ, LL_PAUSE_ENC_RSP, LL_VERSION_IND, LL_REJECT_IND, LL_SLAVE_FEATURE_REQ, LL_CONNECTION_PARAM_REQ, LL_CONNECTION_PARAM_RSP, LL_REJECT_IND_EXT, LL_PING_REQ, LL_PING_RSP, LL_LENGTH_REQ, LL_LENGTH_RSP, LL_PHY_REQ, LL_PHY_RSP, LL_PHY_UPDATE_REQ

Reference Packet

Packet Type

Display the type value of Bluetooth low energy wireless technology packet.

TxAdd

Range: 0 to 1

Default: 0

Set the public state of advertiser's address in Bluetooth low energy wireless technology packet.

RxAdd

Range: 0 to 1

Default: 0

Set the public state of initiator's address in Bluetooth low energy wireless technology packet.

LLID

Set logical link to which the packet belongs.

NESN

Range: 0 to 1

Default: 0

Set the sequence number of next expected packet from the peer Bluetooth low energy wireless technology device in the LL connection.

SN

Range: 0 to 1

Default: 0

Set the sequence number of the Bluetooth low energy wireless technology packet. In multiple packet distribution mode, the SN bit will be set automatically. If a new packet is sent, the value of SN will be toggled.

MD

Range: 0 to 1

Default: 0

Set the more data indication bit of the Bluetooth low energy wireless technology packet.

Include Header Byte

Choice: True | False

Default: True

Double-click or use the drop-down menu to set header byte state of the Bluetooth low energy wireless technology packet.

Header

Range: 0x00 to 0xff

Default: 0x00

Set the header byte of the Bluetooth low energy wireless technology packet.