This topic describes the software's instrument-control properties for the following signal generator models:
N5172B EXG and N5182B MXG
N5166B CXG
E8267D PSG
M9381A
M9420A/M9421A VXT
M9383B VXG-m, M9384B VXG
To open the property grid, click Instrument in the software's tree view. If you are connecting to multiple instruments, the tree view displays a node for each.
The figure below shows the available property categories for a signal generator connection. Click the image links for detailed descriptions.
Click this button to send the parameters to the connected instrument.
Click this button to retrieve the parameters from the connected instrument.
Click this button to set the signal generator to a factory-defined or user-defined state.
Refer to the signal generator's user's guide for information on setting a user-defined state.
Click the DC Cal button to execute an I/Q DC calibration to minimize errors associated with offset voltages.
DC Cal minimizes I/Q offset errors for a single frequency only and must be repeated if the signal generator's settings change.
Download a waveform to set the correct parameters for the target instrument and activate this button.
Click the Power Search button to execute a manual power search calibration. This is an internal calibration routine that improves output power accuracy when the ALC is turned off. A power search is recommended for pulse-modulated signals with pulse-widths less than two microseconds.
Download a waveform to set the correct parameters for the target instrument.
Select the Hint checkbox then click a parameter cell to display a brief description of the parameter.