This window allows you to set the modulation type, boost level and payload for two users. The modulation choices come from the list in the Constellation Settings dialog, which means you can also define your own constellations. The constellation shown in this window is the combined constellation of two users.
Displays the user number. Two users total: 0 and 1.
Choices: BPSK | QPSK | 8PSK |16QAM | 32QAM | 64QAM | 128QAM | 256QAM | 512QAM
Default: QPSK
Set the modulation type.
Range: 0.1 to 10
Default: 1.00
Set the amplitude boost level for current NOMA user.
Choices: PN9 | PN15 | PN23 | Custom Bit Pattern | User File
Default: PN9
Opens the
Data Setup editor to configure payload bits.You can also load, save, and create custom bit patterns.
Range: 0 to 1000
Default: 0
Set the data offset of the payload data.