Fast Information Group

As illustrated in the DAB carrier setup, the FIC is made up of FIBs, and the general structure of the FIB is shown in the figure below. The FIB contains 256 bits and comprises an FIB data field and a CRC.

Figure1: Structure of the FIB

Add a FIG

Select one item of the FIG information, shown as follows.

Delete a FIG

Delete one item of the FIG information.

Up

Move the item (with the arrow on the left) up, one row each time.

Down

Move the item (with the arrow on the left) down, one row each time.

Clear

Clear all the FIG information.