This example shows you how to set up the equipment and configure the N7612C Signal Studio for TD-SCDMA/HSPA 2018 software to create a multi-carrier TD-SCDMA waveform in Basic Capability for a typical Downlink ACLR (Adjacent Channel Leakage Ratio) measurement for component test application. The parameters used in this example are based on the 3GPP TS 25.142 parameters requirement of the BS transmitted signal for ACLR testing.
In this example, an N5182A MXG signal generator is used to achieve the best ACLR performance and the Signal Studio for TD-SCDMA/HSPA software generates the waveform based on the waveform, carrier, timeslot/channel parameters configuration, then download the waveform into the signal generator.
Click in the tree view (left pane of the main window) to configure waveform parameters. The parameter view (right pane) now displays the Carrier Configuration Summary table and the Waveform Setup section. The Waveform Setup section contains the key waveform related parameters.
Add 6 Basic Carriers: You have the option of adding either a Basic or Advanced carrier to the current carrier selection showing in the configuration summary table.
In
the configuration summary table, click the Add new carrier button
.
Select from the drop-down menu.
Repeat step b several times to make sure you have a total of six Basic Carriers listed in the table.
Click the Adjust the frequency offset automatically
button
to allocate the six carriers evenly on the spectrum.
Set the waveform parameters:
: Set the waveform name as desired. The name you define here is displayed on the signal generator when you download the waveform.
: Set to 3 for this example so that the TS4, TS5 and TS6 are downlink timeslots.
: Select Root Raised Cosine, set Alpha = 0.22, Length = 64 symbol for this example. You can set other filter types as desired.
Leave all other parameters settings at their default values.
Now you can see the
six basic
carriers
displayed in the tree view. Click each carrier in the tree view to set
the parameters for that carrier. The Carrier Setup in the parameter view
displays the baseband and 3GPP parameters for that carrier.
: For each carrier, set the SYNC-DL ID as below. Note that the SYNC-UL ID, Scrambling Code and Basic Midamble Code belong to the code group determined by the SYNC-DL ID and change automatically as the SYNC-DL ID changes.
|
|
SYNC-DL ID |
SYNC-UL ID |
Scrambling Code |
Basic Midamble Code |
|---|---|---|---|---|
|
Carrier0 |
0 |
0 |
0 |
0 |
|
Carrier1 |
1 |
8 |
4 |
4 |
|
Carrier2 |
2 |
16 |
8 |
8 |
|
Carrier3 |
3 |
24 |
12 |
12 |
|
Carrier4 |
4 |
32 |
16 |
16 |
|
Carrier5 |
5 |
40 |
20 |
20 |
Leave all other parameters settings at their default values.
For each carrier, click each timeslot under that carrier in the tree view to configure the timeslot parameter. Enable the states of the downlink timeslots TS0, TS4, TS5, TS6.
Enable the state of the Downlink Pilot Timeslot (DwPTS) and disable the state of the Uplink Pilot Timeslot (UpPTS).
Leave all other parameters setting at their default values for each timeslot in each carrier.
Click each timeslot in the tree view to configure the Resource Unit Allocation. The parameter view now displays the Resource Unit Setup tables.
For TS0, TS4, TS5 and TS6, Enable (
) the state for RUs index from 1 to 8.
For TS1, TS2, TS3, make sure all of the RUs States are off.
Leave all other parameters setting at their default values for each RU in the timeslot.
Repeat the above configuration for all of the carriers.
Click in the tree view. The parameter view now shows seven panes: Configuration, Basic, I/Q, ALC, Dual ARB, Dual ARB Marker Utilities, Dual ARB trigger.
: Under Basic Pane, set it to 2 GHz.
: Under Basic Pane, set it to -12 dBm for this example
Multi carrier signals have higher crest factors than single carriers. The output of the signal generator is now spread over multiple carriers thus lowering the carrier level relative to the single carrier case. This phenomena results in multi-carrier signals having lower dynamic range.
Click the Generate a waveform button
in the tool bar. The software generates an
I/Q waveform file in accordance with the current waveform configuration
and signal generation setup. Waveform generation time varies proportionally
to the complexity of the waveform.
After the waveform is generated, you can examine its characteristics.
View the CDP graph for each carrier based on the configuration by clicking the carrier in the tree view. For more information, refer to CDP Graph.
By clicking the in the tree view, you can view plots of the baseband spectrum, I and Q signals, and CCDF curve prior to downloading the file to the signal generator. For more information, refer to CCDF Graph and Waveform Graph.
To download the waveform file to the signal generator,
click Download
in the tool bar if you have configured the instrument connection.
The signal generator automatically begins to play the TD-SCDMA waveform.
Local control of the signal generator is re-enabled by pressing the hardkey, allowing signal generator
settings to be modified from the front panel. The waveform file, however,
cannot be modified after downloading it to the signal generator.