This topic describes the CCDF functionality using the graph in the Waveform Setup view. Clicking Waveform Setup under the tree view to display the CCDFgraph.
The CCDF graph displays the probability (in percentage) of the generated waveform's calculated peak-to-average power ratio (measured in dB) meeting or exceeding a certain level. The table to the left of the CCDF plot displays the calculated peak-to-average values for the current waveform. For additional information, see Understanding CCDF Curves.
Click
or
from the main
tool bar to generate an I/Q waveform and plot the
CCDF graph using the current channel configuration.
Any changes to the channel configuration setup do not appear on the graph
until you generate the waveform. The status bar at the bottom of the screen
shows waveform generation progress.
The CCDF and Waveform graphs
are minimized in the Waveform Setup node's initial view. To view the graphs,
click and drag the
border
above the CCDF and Waveform graphs.
Each time you adjust parameters and generate a waveform, a plot is added
to the
graph.
The graph retains your three most recent plots (in shades of gray), allowing
you to make comparisons of waveform characteristics.
Use the buttons shown below to plot the Gaussian data, reference data and generated waveform data to the CCDF graph. The graph's initial state shows only the Gaussian curve (blue) until you generate a waveform.
Click to toggle the view of the band-limited Gaussian noise curve (blue).