Arbitrary Waveform Generator

1. Configuration 2. Basic 3. Output

Address

Instrument

Sample Rate

Filter

Trigger Source

Trigger Delay

Trigger Slope

Trigger Level

State

Load

Dual Channel Operation

Voltage

Voltage Offset

Peak Voltage

Voltage Limits

Voltage High Limit

Voltage Low Limit

1. Configuration

Address

Enter the instrument address.

The drop down list of Address lists the recently used instrument address and the connection strings (GPIB, USB, LAN, and so on) configured in Keysight IO Connection Expert.

Instrument

Default: 33522B

2. Basic

Sample Rate

Range: 1 Hz to Maximum sample rate supported by the instrument, which is 1 GHz for 33622A, 250 MHz for 33522B

Default:

PA Test: 15 MSa/s

Dual-band PA Test: 60 MSa/s

Set the sample rate of the Envelope Signal Generator. By default, this value is set to three times of the product of the Sample Rate value and Resampling Ratio value in Waveform block and the OSR for Envelope value in Envelope Tracking block.You can set it to a larger value if you like.

Filter

Choice: Normal | Step |Off

Default: Normal

Specifies the filter setting for an arbitrary waveform.

Trigger Source

Choice: External | Bus

Default:

PA Test: Bus

Dual-band PA Test: External

Coupling: Trigger Source will be coupled to External if the Trigger Master setting in the Envelope Tracking block is set to RF Signal Generator, and will be coupled to Bus if the Trigger Master setting in the Envelope Tracking block is set to Envelope Signal Generator.

Set the type of trigger source of the Envelope Signal Generator.

Trigger Delay

Range: 1 ns to 1ks

Default: 0 s

Coupling: If Envelope Tracking block is set to On and the Trigger Master in Envelope Tracking block is set to RF Signal Generator, this setting and the I/Q Delay setting in RF Signal Generator block will be determined by the Delay value in the Envelope Tracking block.

Set the trigger delay of the Envelope Signal Generator.

Trigger Slope

Choice: Rising | Falling

Default: Rising

Set the polarity of the Envelope Signal Generator's external trigger. If the Trigger Source is set to Bus, this setting is read-only.

Trigger Level

Range: 900 mV to 3.8 V

Default: 3.3 V

Coupling: Available only when the envelope signal generator is 33622A.

Set the trigger level of the Envelope Signal Generator's external trigger. If the Trigger Source is set to Bus, this setting is read-only.

3. Output

State

Choice: On | Off

Default: On

Double-click or use the drop-down menu to turn on or turn off the output of the Envelope Signal Generator.

Load

Choice: 50 Ω | 100 Ω | High-Z

Default: 50 Ω

Double-click or use the drop-down menu to set the output load.

Dual Channel Operation

This parameter displays the current Dual Channel Operation Status. For N7614C Signal Studio for Power Amplifier Test 2022, the value is Inverted.

Voltage

Range: 0 to 7.5658 V for 33522B, 10 V for 33622B

Default: 0 V

Coupling: This value is coupled with the calculated peak to peak value of VREF.

Set the output voltage.

Voltage Offset

Range: -4.99950 V to 4.99950 V

Default: 0 V

Coupling: This value is coupled with the Vcm value in ETPS block.

Set the output voltage offset.

Peak Voltage

Range: 0.1 to 1.1 v

Default: 0.4

Coupling:

Set the peak voltage of the envelope signal generator. Refer to Voltage Mapping in Envelope Tracking Measurement for more details about peak voltage.

Voltage Limits

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to turn on or turn off the voltage limits.

Voltage High Limit

Range: -4.999 V to 5 V

Default: 5 V

Set the output voltage high limit.

Voltage Low Limit

Range: -5 V to 4.999V

Default: -5 V

Set the output voltage low limit.