Example Wideband DPD Measurement

To support digital pre-distortion (DPD) testing on wideband signals like wideband WLAN (802.11ac 80 MHz/160 MHz), the N7614C Signal Studio for Power Amplifier Test 2022 software supports playing the wideband arbitrary waveform on an M8190A arbitrary waveform generator with an external IQ connection to an E8267D PSG.

The whole measurement process includes the following four parts.

  1. Setting up the measurement system

  2. Calibrating the RF Signal Generator (M8190A+PSG)

  3. Configuring parameters in the N7614C software

  4. Executing the measurement and viewing results

Return to the Tutorials menu.