When Signal Studio is used to download and initiate waveform playback in multiple instruments, it sends SCPI commands to set up the triggering parameters and initiate the waveform playback so that the playback starts at the same time in each instrument. If you choose to store waveforms in the instruments and recall them for playback from the instrument memory, rather than using Signal Studio directly, additional steps are needed to get synchronized waveform playback. The front panel keystrokes in the procedure below can be replaced by SCPI commands in a software program.
First, connect the instruments as shown in the Tutorials section of the online help for your desired configuration:
Multiple Antennas Solution Without Baseband Timing Alignment and RF Phase Coherence
Multiple Antennas WiMAX Solution With Baseband Timing Alignment, but Without RF Phase Coherence
Multiple Antennas WiMAX Solution With Baseband Timing Alignment and RF Phase Coherence
Make sure that the EVENT 2 output of the master ESG/PSG is connected to the PATT TRIG IN 1 connectors on both the master and slave ESGs/PSGs. The 10 MHz references should be connected between the instruments.
For each instrument, press these keys: > > > > > > and verify that Patt Trig In 1 is selected. Next, press > and set this to Trigger & Run. This will set up the instrument to start playing back the waveform continuously when it receives an external trigger input on the PATT TRIG IN 1 connector, and to ignore further trigger signals.
On each instrument, select the desired waveform, but leave the ARB turned off:
Press > > , select and load the desired segment(s).
Press > , and select the desired waveform file.
Send the following SCPI commands to the master ESG or PSG to prepare it to output periodic triggering pulses on the EVENT 2 output. If you are not using a software program to control the test, you can use the Keysight Connection Expert to connect to the instrument and send the following SCPI commands:
diag:bbg:mon "ww a6000004 30"
diag:bbg:mon "ww a6000058 6000"
diag:bbg:mon "ww a600005c 6001"
Turn on the ARB in each instrument: > > (if needed). Set the desired frequency and amplitude for the output signal and turn RF on. See Power Settings for N7615C Signal Studio for Mobile WiMAX for information about setting N7615C waveform power.
Send these SCPI commands to the master ESG or PSG to generate the trigger pulses to start the waveform playback and to stop the pulse generation. No delay is needed between the commands since the hardware works faster than the SCPI command processing.
diag:bbg:mon "ww a6000056 3"
diag:bbg:mon "ww a6000056 0"
Turning off the ARB on any of the instruments will cause a loss of synchronization. To re-synchronize the waveform playback or change to a different waveform(s), repeat steps 2-5.
Make sure that the EVENT 1 output from the master MXG/EXG is connected to the PAT TRIG IN on the slave MXG/EXG. The 10 MHz references should be connected between the instruments.
You can use multiple N5182A signal generators in the same system, or you can use N5172B and N5182B signal generators in the same system. However, you cannot use a mixture of N5182A signal generators and N5172B or N5182B signal generators in the same system.
If you are using an N5172B or N5182B and one or more N5182A signal generators, you must configure the N5172B or N5182B as the Master. In addition, the N5182A slaves must be at the end of the instrument chain.
On the master MXG/EXG, press these keys to set up the trigger type, trigger mode, and trigger source: > > > > > > > . Here you can choose , , or as the trigger source. is convenient for manual operation. trigger can easily be sent with a SCPI command so that is a good choice if the measurement is automated. uses an external trigger signal applied to Patt Trig In 1 (by default), which is the PAT TRIG rear panel connector.
If was selected for the Trigger Source, disconnect the external trigger signal from the PAT TRIG input on the master MXG/EXG.
On the slave MXG/EXG(s), press these keys to set up the trigger type and trigger mode. The default trigger source of Patt Trig will be used: > > > > > . Press these keys to verify that the trigger source is set to , with External defined to be the rear panel Patt Trig In 1 input: > > > > > .
Press these keys to set up the master MXG/EXG for the Multi-BBG Sync function: > > > > > > then
for a N5182A master, set as appropriate.
for an N5172B or N5182B master, set and as appropriate.
On each slave MXG/EXG, press these keys to set up the Multi-BBG Sync function: > > > > > > then
for a N5182A slave, set and as appropriate.
for an N5172B or N5182B slave, set , , and as appropriate.
On each slave MXG/EXG, press .
On the master, press . The status on all MXG/EXGs should show .
In each MXG/EXG, select the desired waveform file and turn Arbs ON: > > > to load the waveform files into the baseband generator memory if needed, then highlight the desired waveform file and press > . Set the desired frequency and amplitude for the output signal and turn RF on. See Power Settings for N7615C Signal Studio for Mobile WiMAX for information about setting N7615C waveform power
Initiate the waveform playback using one of these steps, depending on which Trigger Source was selected in step 1:
Trigger Source = Trigger Key: press to start the waveform playback.
Trigger Source = Bus: Send the *TRG SCPI command to the master MXG/EXG. If you are not using a software program to control the test, you can use the Keysight Connection Expert to connect to the instrument and send the SCPI commands.
Trigger Source = Ext: Connect the external trigger signal to the PAT TRIG input on the master MXG/EXG.
To change waveforms or resynchronize the MXG/EXGs:
If using an external trigger for the master MXG/EXG, disconnect it or turn it off.
Turn off all of the ARBs by pressing > > and press > > on each MXG/EXG.
Repeat steps 6 through 9.
When two instruments are directly controlled by the N7615C Signal Studio
software, you set the desired amplitude for the master instrument, but
Signal Studio will automatically set the amplitude on the slave instrument
to get the correct output power for the Antenna 1 signal (see Power Settings for more information).
When Signal Studio is not used to directly download the waveforms and
control the Instruments, you are responsible for selecting the correct
amplitude setting for the slave instrument. Keysight recommends that you
make a note of the relative power settings for the master and slave instruments
when you first create and download each set of waveform files. The amplitude
settings can be found by clicking on Instrument in the
tree view
after the waveform files have been generated. You can also save the instrument
state in the instruments for later use by creating a Quick Setup.