Waveform Download Problems

License Errors

If you attempt to download a waveform and the waveform license is not found or is expired, an error message displays in the status bar and the status window. See Licensing for information on resolving license errors.

Download Takes a Long Time

If the instrument connects directly to the PC using a crossover LAN cable and downloading a waveform takes a long time, or there are connection problems even if the ping command is successful, add the instrument's IP address and hostname to the Hosts file. The Hosts file is a common way to map a hostname to an IP address. (For more information on Hosts files, go to www.microsoft.com and search on "example hosts file.")

Depending on the operating system, you will find the Hosts file in one of the following directory paths:

C:\Winnt\System32\Drivers\Etc\

C:\Windows\System32\Drivers\Etc\

Procedure

  1. In a text editor such as Notepad, open the Hosts file.

  2. Write the IP address for the instrument at the bottom of the file. (Refer to the example of a hosts file below.)

  3. Save the file and close the text editor.

Do not use "Save As" when saving the Hosts file; this file does not have a file extension.

Example Hosts File 

# Copyright (c) 1993-1999 Microsoft Corp.

#

# This is a sample HOSTS file used by Microsoft TCP/IP for Windows.

#

# This file contains the mappings of IP addresses to host names. Each

# entry should be kept on an individual line. The IP address should

# be placed in the first column followed by the corresponding host name.

# The IP address and the host name should be separated by at least one

# space.

#

# Additionally, comments (such as these) may be inserted on individual

# lines or following the machine name denoted by a '#' symbol.

#

# For example:

#

# 102.54.94.97 rhino.acme.com # source server      

# 38.25.63.10 x.acme.com # x client host           

<xxx.xxx.xxx.xxx> localhost

<xxx.xxx.xxx.xxx> <instrument hostname>

Equipment Setup and Connection

Software Problems

Interface Problems

Instrument Problems

Contacting Keysight