Installation Steps: 1 2 3 4 5 6 7
A Microsoft .NET Framework version may come pre-installed with your Windows operating system. If the pre-installed .NET Framework version is not the same version as stated in the text below, you must install the required version. Different versions of .NET Framework can simultaneously reside on the Windows operating system.
Ensure that you have Microsoft .NET Framework 3.5, or .NET Framework 3.5 Service Pack 1 installed on the Windows operating system (PC or Windows-based instrument) that is to receive the Signal Studio software download. If you know it is already installed, proceed to Installation Step 3.
With Windows 8.1 you do not have to install .NET Framework, rather you enable it in the Control Panel and it is downloaded and installed automatically. You must perform this procedure as the administrator and be connected to the internet.
Go to > > > .
Windows Featuresdialog box appears, indicating the state of .NET Framework 3.5. Make sure the checkbox is marked.Press . This will begin the installation process of .NET Framework 3.5.
.NET Framework 3.5 is included with Windows 7, but you can verify it is turned on by doing the following:
Go to > > > > .
Windows Featuresdialog box appears, indicating the state of .NET Framework 3.5.If you do not have the .NET Framework 3.5 installed, do the following:
Search the site for .NET Framework 3.5.
Download and install the software.
If you get a security exception message when you try to open the software, consult your system administrator to resolve the problem.