6. Equipment Setup and Connection

Installation Steps: 1 2 3 4 5 6 7

Some instruments require unique configurations for use with Signal Studio and are not described in this topic. In these cases, refer to Tutorials for specific information on how to configure your instrument.

Connecting to a signal generator

  1. Ensure the signal generator is turned off.

  2. Connect the signal generator to the computer using one of the following methods for instrument control:

Connecting to a PXB

This section only applies if you are connecting a PC to the PXB. If you are using the PXB as the controller, no connections are required and you can ignore this section.

  1. Ensure the PXB is turned off.

  2. Connect the PXB to the computer using one of the following methods for instrument control. See the PXB's online documentation for GPIB and LAN configuration information.

Tutorials