Installation Steps: 1 2 3 4 5 6
Ensure the equipment is turned off.
Connect the equipment to a computer using one of the following methods for instrument control:
LAN
Network—
connect
the hardware and computer to an
external LAN network using standard LAN cables.
If you are connecting to an E6640A, the instrument has two (2) LAN ports on the front panel. LAN 2 (the left most port) uses a static assigned IP address, and you should use the LAN 2 port to connect the test set.
Crossover
LAN—
connect
the hardware directly to the computer using a crossover LAN cable.
(You will need to configure your PC using this setup.)
If you are connecting to an E6640A, the instrument has two (2) LAN ports on the front panel. LAN 2 (the left most port) uses a static assigned IP address, and you should use the LAN 2 port to connect the test set.
Crossover
LAN—If
connecting
more than one instrument (signal generator, spectrum analyzer):
one 10Base-T crossover cable for the PC
one 10Base-T cable for each instrument
one 10Base-T hub
GPIB—
connect
the equipment directly to the computer
using a GPIB cable.
PXI—connect the computer's MXI/PXI adapter to the PXI mainframe.
The following hardware can be used to create a system:
|
Signal Generator |
E4438C |
|
E8267C |
|
|
E8267C Option 015 |
|
|
E8267D |
|
|
E8267D Option 015 |
|
|
N5172B |
|
|
N5182A |
|
|
N5182B |
|
|
Baseband Generator and Channel Emulator |
N5106A |
|
Wireless Communications Test Set |
E6607 |
|
Wireless Test Set |
E6640 |
|
Arbitrary Waveform Generator |
ESG/PSG Internal AWG (Options 001, 002, 601, 602) |
|
N5172B Internal AWG |
|
|
N5182A/B Internal AWG |