Downloading the waveform places the signal generator in the remote operation mode and deactivates front panel operation. On the signal generator, press the key to restore front panel operation.
Check the signal generator for error messages; if possible, correct the conditions indicated by the messages.
When a setting conflict (error) occurs, an error number and a brief message appear at the bottom of the signal generator display. To view the full text of the error messages use the method shown for your instrument:
ESG:
Press on the signal generator front panel to view error messages on the display.
Execute the SCPI error commands described in the System Subsystem section of the SCPI Reference manual.
MXG/EXG:
Press the hardkey on the signal generator front panel to view error messages on the display.
(For the MXG ATE, use the web interface.)
PSG:
Press on the signal generator front panel to view error messages on the display.
Execute the SCPI error commands described in the System Subsystem section of the SCPI Reference manual.
Refer to the instrument's documentation for further troubleshooting information.
Contact a Keysight Technologies Service Center.
This error is displayed when the PXB is not configured to accept an ARB waveform file or if not enough BBG resources are available. Check the following possible causes:
Confirm that you have loaded the correct configuration on the PXB.
Confirm that the loaded configuration contains the correct number of BBGs. For example, if Signal Studio set up to download two waveform files for 2X2 MIMO, the loaded PXB configuration must contain at least two BBGs.
You cannot download waveforms from Signal Studio to the PXB while the PXB is playing a waveform.
Press the ”Stop” button on the PXB to stop the currently playing waveform before downloading waveforms from Signal Studio.
Refer to the PXB's online documentation for more error message descriptions and troubleshooting procedures.
Verify that the equipment meets the minimum requirements. See System Requirements.
Refer to the computer's documentation for troubleshooting and repair.