Selecting in the
tree view
to display a list of waveform setups, each of which is associated with
a specific user-defined hardware configuration or a predefined hardware
configuration (SimHW).
Quick setups are accessible only from the Quick Setup node in the user interface. To save your waveform setup as a file that can be shared with other users, use > or > .
You can use the System Configuration Wizard to start a new setup using actual hardware, or you can choose from predefined setups using simulated or actual hardware. You can customize the settings and save as a quick setup for later use. Quick Setups saves the Instrument and Waveform Setup parameters.
Signal Studio software provides predefined quick setups that enable you to examine the default parameters for a particular function, while in simulated hardware mode. You can use the predefined quick setups as a starting point, modify the settings as desired, then save them as a new quick setup (see Custom Quick Setup). However, you cannot modify or delete the predefined quick setups.
If you install the Signal Studio for Digital Video software on the PXB, the following predefined quick setups are available if you have selected as the Custom Setup during installation. These quick setups include actual hardware configurations (not simulated hardware settings) and waveform settings for typical Digital Video use cases on your PXB.
After you have defined waveform parameters in the Instrument node and the Waveform Setup node, you can associate this waveform setup with the currently configured hardware (displayed in the Hardware node) by pressing the button and providing a name for the new Quick Setup.
To save the current waveform setup with a different hardware configuration, define the new hardware configuration using the System Configuration Wizard ( > ), then click .
If you change one or more Waveform Setup parameters, the software prompts you to save the changes as a Quick Setup when you exit. If you have changed only Hardware node or Instrument node settings, the software does not prompt you to save changes when you exit. Use the button to save these changes to a Quick Setup
Use the following buttons to manage your quick setups:

Click this button to save the current hardware system and software configuration
as a custom quick setup. A
window
appears, enabling you to enter a name for the quick setup.
To save only Hardware parameter changes, you must use the Save As Quick Setup button. You are not prompted to save Hardware parameter changes when closing or exiting the software unless changes are also made to the Waveform Setup.

Click this button to open the selected quick setup. Double-clicking the quick setup performs the same function.

Click this button to delete the selected custom quick setup.