The software controls PUCCH transmission based on the subframe status as set in the UCI Subframe Settings tab. The DMRS for PUCCH are assigned according to the PUCCH format and the cyclic prefix mode.
The software does not use these settings when it is controlling multiple instruments as shown in the tree view.
|
1. PUCCH Settings |
2. Transmission Settings |
3. Demodulation Reference Signal Settings |
|---|---|---|
|
|
|
|
|
|
|
References:
3GPP TS 36.211 Physical Channels and Modulation:
5.4 Physical uplink control channel
|
|
This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. When using multiple instruments as shown in the tree view, this button is not displayed. |
|
|
This button displays in place of the Settings Current button. It indicates that the instrument settings are not currrent and need to be updated with the new software settings. Click this button to update the insturment's settings. This button shows in all windows regardless of where the change was made. When using multiple instruments as shown in the tree view, this button is not displayed. |
Choice: On |Off
Default: On
Coupling: This setting is inactive and set to off when using multiple instruments as shown in the tree view.
Sets the PUCCH channel state.
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh[:STATe] 0|1|OFF|ON
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh[:STATe]?
Range: -60 to 20
Default: 0
Sets the PUCCH channel power in dB.
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:POWer <val>
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:POWer?
Range: 0 to <maximum or resource blocks - 1>
Default: 0
Sets the bandwidth in terms of resource blocks,
, that are available for use by formats 2, 2a, 2b transmission in each slot. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see TS 36.211).
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:NRB2 <val>
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:NRB2?
Range: 0 to 7
Sets the number of cyclic shifts,
, for formats 1/1a/1b used in a resource block with a mix of formats 1/1a/1b and 2/2a/2b. There is at most one mixed resource block per slot. No mixed resource block is present if this value is 0. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see TS 36.211).
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:NCS[1] <val>
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:NCS[1]?
|
Range: |
||
|
0-215 |
1.4 MHz BW |
|
|
0-539 |
3 MHz BW |
|
|
0-899 |
5 MHz BW |
|
|
0-1799 |
10 MHz BW |
|
|
0-2699 |
15 MHz BW |
|
|
0-3599 |
20 MHz BW |
|
|
|
|
|
|
0-143 |
1.4 MHz BW |
|
|
0-359 |
3 MHz BW |
|
|
0-599 |
5 MHz BW |
|
|
0-1199 |
10 MHz BW |
|
|
0-1799 |
15 MHz BW |
|
|
0-2399 |
20 MHz BW |
|
Default: 0
Sets the resource index,
, for PUCCH Formats 1, 1a, 1b.
The maximum value (the range of values) is calculated by the system bandwidth, cyclic prefix, N_RB(2), N_CS(1) and Delta Shift. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS 36.211).
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:N[1] <val>
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:N[1]?
Sets the resource index,
, for PUCCH formats 2, 2a, 2b, expressed in multiples of
, the resource block size expressed as a number of subcarriers. This is mapped directly into a single cyclic shift resource. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS 36.211).
Range:
Default: 0
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:N2 <val>
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:N2?
The demodulation reference signals are defined by a cyclic shift and use the same resource allocation used by PUCCH; power can be set independently. The DMRS for PUCCH are assigned according to the PUCCH format and the cyclic prefix mode. For example, when the PUCCH format is 1/1a/1b with normal cyclic prefix, the DMRS for PUCCH is assigned to SC-FDMA symbols #2, #3, and #4 in a PUCCH slot.
Range: -60 to 20
Default: 0
Sets the power in dB of the demodulation reference signal (DMRS) for PUCCH relative to the carrier power.
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:DMRSignal:POWer <val>
[:SOURce]:RADio:LTE:FDD[:BBG]:ULINk:PUCCh:DMRSignal:POWer?
Choices: 1 | 2 | 3
Default: 1
Enter the Delta Shift
, the number of equally spaced cyclic time shifts. This parameter is used in calculating the number of DMRS PUCCH resources per resource block reserved for DMRS.