Click  or  in the 
tree view. 
 The graph view is located at the bottom of the Waveform Setup and Carrier 
 nodes, and in the Waveform Library Manager's Library Manager window (i.e. power 
Spectrum view only). For multiple antenna configurations, a tab for each antenna port 
 is displayed above the graph view. Click the tab of the antenna port for 
 which you want to view a waveform graph. Click the Waveform tab to display 
 the waveform graph. 
The CCDF, Waveform, and Power Envelope graphs are minimized 
 in the initial view of the Waveform Setup node and the Carrier node. To 
 view the graphs,        
click and drag the border 
 above the CCDF, Waveform, and Power Envelope  graphs.
Click  
or 
  
 
 from the main tool bar to generate an I/Q waveform and plot four different 
 waveform graphs (Power, I+Q, I/Q, and Spectrum) of 
 the current waveform configuration. Changes to the waveform configuration 
 do not appear on the graph until you generate the waveform. The status 
 bar at the bottom of the screen shows waveform generation progress.
The plot is shown in the Figure.
            
        
Figure. Power plot
Click the down arrow 
 to open a 
drop-down menu 
 from which you can select different waveform plots. Selections include 
 Power (shown above), I+Q, I|Q, and 
 Spectrum. Click the button to the left of the arrow 
 to select the next plot type in the list 
 without displaying the menu.