Real Time

Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Multi-UE Wizard

This window provides all the functions necessary to configure a multi-UE waveform and is accessed by clicking the Multi-UE Wizard button in the Waveform Setup screen. When you have finished your configuration, click OK and a small Closedprogress window appears briefly as the software checks for resource block conflicts. An error message reports the details should any conflicts occur. Otherwise, the configuration is valid.

Open Multi-UE Wizard Settings

Opens a multi-UE settings file (*.mus). Also supports *.txt and *.csv file formats. Refer to Importing and Exporting Multi-UE Settings Files for more information.

Save Multi-UE Wizard Settings

Saves your current configuration to a multi-UE settings file (*.mus). Also supports *.txt and *.csv file formats. Refer to Importing and Exporting Multi-UE Settings Files for more information.

Preset Multi-UE Wizard Settings

Presets the multi-UE wizard to the default configuration.

Carrier Type

Displays the UL carrier that is fixed at Advanced LTE UL.

System BW

Choice: 1.4 MHz (6RB) | 3 MHz (15RB) | 5 MHz (25RB)) | 10 MHz (50RB) | 15 MHz (75RB) | 20 MHz (100RB)

Default: 10 MHz (50RB)

Double-click or use the drop-down menu to set the system bandwidth and number of Resource Blocks (RB). When you select a system bandwidth, the software automatically adjusts the value in the Total number of Resource Blocks cell and the Total number of Occupied Sub-carriers cell.

Cell ID

Range: 0 to 503

Default: 0

Enter a value of the cell ID for Multi-UE Generation. See 3GPP TS 36.211 for more information.

Generation Length

Range: 10 ms to 160 ms

Default: 10 ms

Enter a value of waveform generation length.

Number of UEs

Range: 1 to 100

Default: 25

Enter a number of UEs signal for Multi-UE Generation.

PUSCH

Displays the PUSCH state. A check mark indicates the channel is on.

PUSCH

This table shows the configurations for each individual UE. UE parameters can be set independently or globally, using Column Preset.

Column Preset

This button opens a drop-down menu, allowing you to select a global setting for a certain UE parameter.

UE #

Displays the UE number.

RNTI

Range: 0 to 65535

Default: 0

Enter a value for the Radio Network Temporary Identifier (RNTI).

MCS Index

Choice: Off | 0 | 1 ..... 26 | 27 | 28

Default: 0

Double-click or use the drop-down menu to set the MCS index of MCH. In case of MCS Index = 0 to 28, both parameters Modulation and TBS Index are automatically decided by software. In case of MCS Index = Off, both parameters Modulation and TBS Index are selectable by user. For more detail, refer to 3GPP TS 36.212, 36.213 and 36.331.

HARQ-ACK

Choice: On | Off

Default: Off

Sets HARQ-ACK state on or off.

HARQ-ACK Offset Index

Range: 0 to 15

Default: 0

Enter a value for the HARQ-ACK Offset Index.

HARQ-ACK Info

Choice: ACK | NACK | ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK | User Defined Bits (Up to 0 to 20 Bits)

Default: ACK

Sets HARQ-ACK Information. If User Defined Bits is selected, Bit sequence containing "0" or "1" up to 20 bits is available. "1" means ACK. "0" means NACK.

HARQ-ACK Info Size

Range: 1 to 20

Specifies HARQ-ACK Information Size. If HARQ-ACK Info is set User Defined Bits, HARQ-ACK Information Size is available to set up to User Defined Bits length. Otherwise it is read only.

RI

Choice: On | Off

Default: Off

Sets RI state on or off.

RI Offset Index

Range: 0 to 12

Default: 0

Enter a value for the RI Offset Index.

RI Info

Choice: 0 | 1 | 0-0 | 0-1 | 1-0 | 1-1 | User Defined Bits (Up to 0 to 15 Bits)

Default: ACK

Sets RI Information. If User Defined Bits is selected, Bit sequence containing "0" or "1" up to 15 bits is available.

RI Info Size

Range: 1 to 15

Specifies RI Information Size. If RI Info is set User Defined Bits, RI Information Size is available to set up to User Defined Bits length. Otherwise it is read only.

CQI/PMI

Choice: On | Off

Default: Off

Sets CQI/PMI state on or off.

CQI Offset Index

Range: 2 to 15

Default: 2

Enter a value for the CQI Offset Index.

CQI/PMI Info

Choice: PN9 | PN15 | User Defined Bits

Default: PN9

Sets CQI/PMI Information.

CQI/PMI Info Size

Range: 1 to 144

Specifies CQI/PMI Information Size.

RB Allocation Graph

Displays how resource blocks are allocated for a specific UE. Click the blank cell to the left of the UE # you want to see in the graph. If you right-click anywhere in the row of the selected UE, a ClosedSet Selected UEs Transmission button appears. Clicking this button opens the ClosedUE #n PUSCH Tx Sequence editor for the UE, allowing you to set subframe states and resource block offsets and sizes (video). To show the RB allocation for all the UEs, click the blank cell to the left of Carrier Type in the upper table of the wizard.