Click in the tree view to display the waveform pane shown below. The waveform setup pane is divided into three sections: Carrier Configuration Summary Table (top), Waveform Attributes Table (middle), and Graph View (bottom).
This table enables you to view the key parameters for each carrier in the waveform. You can also add or delete carriers using the buttons above the table (see descriptions below). Double-click a carrier row to activate the setup tables for that carrier.
An asterisk following a carrier entry
indicates that parameters for the carrier have changed.
Click this button to open a drop-down list from which you can select a carrier to add to the setup table. The carrier is inserted above the currently selected carrier in the table. The maximum number of carriers is 16. You can also make older carrier versions available by clicking View > Show Legacy Carrier from the menu bar.
For Advanced waveforms, if Waveform Generation Length is >160 ms, the Add Carrier and Copy Carrier buttons will not work. Refer to the Carrier n node's topic for Uplink or Downlink. Waveform Generation Length's >160 ms is not available for all 3GPP Advanced waveforms.
Long waveform generation requires N5172B/82B with firmware version ≥B.01.10.
Click this button to delete the currently selected carriers in the setup table. You can highlight multiple carriers by holding down the CTRL key while selecting the carriers. You can also use the SHIFT key to select a succession (group) of carriers.
Click this button to quickly add a copy of the selected carrier to the carrier configuration summary table.
For Advanced waveforms, if Waveform Generation Length is >160 ms, the Add Carrier and Copy Carrier buttons will not work. Refer to the Carrier n node's topic for Uplink or Downlink. Waveform Generation Length's >160 ms is not available for all 3GPP Advanced waveforms.
Long waveform generation requires N5172B/82B with firmware version ≥B.01.10.
This button opens the Mufti-UE Wizard window.
Enter an alpha-numeric waveform file name of up to 22 characters. (If you enter a name with more than 22 characters, the software truncates the name to 22 characters when you click outside of the cell.) The name can include spaces and the following special characters: _ $ & # + - [ ].
Enter an alpha-numeric comment of up to 32 characters. The comment resides in the file header and can include spaces and special characters.
Displays the generated waveform length (number of points). You cannot edit this cell. Waveform length is directly related to the oversampling ratio value selected. (Increasing the oversampling ratio increases the total sample points.)
Choice: Auto | Manual
Default: Auto
Double-click or use the drop-down menu to select the Sampling Rate Mode.
Auto: Sampling Rate is calculated based on each carriers's settings.
Manual: Uses Waveform Sampling Rate value as a target sampling rate.
View or set the sampling rate of generated waveform, depending on the Waveform Sampling Rate Mode setting.
This cell is read only. Waveform Sampling Rate value is calculated based on each carrier settings; Sampling Rate is directly related to the oversampling rate value selected and/or frequency offset value. (Increasing the frequency offset increases the sampling rate.) After waveform generation has finished, value is refreshed and updated.
Range: depends on the target instrument
Default: depends on the target instrument (typically 30.72 Msps)
This cell is editable. The Waveform Sampling Rate value is used as the sampling rate to generate waveform.
Multi-carrier case: Minimum value is the Least Common Multiple (LCM) value of Base Sampling Rate of carriers or instrument's minimum sampling rate. Value should be the multiple of LCM value of Base Sampling Rate values within 30.72 Msps.
Single Carrier case: Minimum value is 1.92 Msps or instrument's minimum sampling rate. Value should be the multiple of Base Sampling Rate within 30.72 Msps, or the multiple of 30.72 Msps over 30.72 Msps.
Range Max: 1000
Range Min: 0.001
Step: 0.00000000000001 (number of decimal places is 14 digits)
Default: 1
Sets the value by which to scale the bandwidth and time lengths of the measured signal. This setting can be used to compensate for mis-tuned crystals or to allow demodulation of signals at a lower rate, such as half rate or 1/10 rate.
Examples:
For a 1/10 rate signal, the Time Scale Factor would be 0.1
For a crystal mistuned by 5 ppm, a value of 1.000005 or 0.999995 could be used
This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U06 or greater is valid. Refer to Licenses for more information.
Double-click or use the drop-down menu to select a normal or inverted I/Q signal.
Displays the raw cubic metric, which can be used for cubic metric (CM) calculation.
This parameter is not available when the MIMO, Tx Diversity, or Inter-band hardware configuration is selected.
This value updates after a successful waveform generation.
Double-click or use the drop-down menu to control the operating state of the digital pre-distortion.
This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U01 or greater is valid. Refer to Licenses for more information.
Double-click or use the drop-down menu to open or close the Digital Pre-Distortion Tool window. This is a modeless window, allowing you access to the main software GUI so you can continue to configure and generate waveforms.
This parameter appears in the software's GUI only when Minor Enhancement Update (MEU) Option U01 or greater is valid. Refer to Licenses for more information.
Displays the multi-UE generation state. Multi-UE generation is performed with the Multi-UE Wizard.
Configure the marker points for Marker 1 using the Marker Source Selection dialog box.
The signal generator outputs the Marker 1 signal from the rear-panel EVENT 1 output. For more information, see the signal generator's User Guide.
Configure the marker points for Marker 2 using the Marker Source Selection dialog box.
The signal generator outputs the Marker 2 signal from the rear-panel EVENT 2 output. For more information, see the signal generator's User Guide.
When Parameter Optimization in the Signal Generator node is set to , the Marker 3 and Marker 4 source selections in the Waveform Setup node and the marker routings selected in Dual ARB Marker Utilities are overridden.
To manually set the Marker 3 and Marker 4 source, the marker routing, or both, set Parameter Optimization to .
Configure the marker points for Marker 3 using the Marker Source Selection dialog box.
The signal generator outputs the Marker 3 signal from the rear-panel EVENT 3 output. For more information, see the signal generator's User Guide.
When Parameter Optimization in the Signal Generator node is set to , Marker 3 and Marker 4 source selections in Waveform Setup node and the marker routings selected in Dual ARB Marker Utilities are overridden.
To manually set the Marker 3 and Marker 4 source, the marker routing, or both, set Parameter Optimization to .
Configure the marker points for Marker 4 using the Marker Source Selection dialog box.
The signal generator outputs the Marker 4 signal from the rear-panel EVENT 4 output. For more information, see the signal generator's User Guide.
The graph view displays several different representations of the generated waveform. For more information, see Graph View.